Microchip® Advanced Software Framework

mlme_get_conf_tag Struct Reference

This is the MLME-GET.confirm message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 < This identifies the message as MLME_GET_CONFIRM More...
 
uint8_t PIBAttribute
 
pib_value_t PIBAttributeValue
 < The value of the indicated MAC PIB attribute that was read. More...
 
uint8_t status
 The identifier of the MAC PIB attribute to get. More...