Microchip® Advanced Software Framework

mlme_orphan_resp_tag Struct Reference

This is the MLME-ORPHAN.response message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t AssociatedMember
 TRUE if the orphaned device is associated with this coordinator or FALSE otherwise. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_ORPHAN_RESPONSE. More...
 
uint64_t OrphanAddress
 The address of the orphaned device. More...
 
uint16_t ShortAddress
 The short address allocated to the orphaned device if it is associated with this coordinator. More...