Microchip® Advanced Software Framework

mlme_reset_req_tag Struct Reference

This is the MLME-RESET.request message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 < This identifies the message as MLME_RESET_REQUEST More...
 
uint8_t SetDefaultPIB
 If TRUE, the MAC sublayer is reset and all MAC PIB attributes are set to their default values. More...