Microchip® Advanced Software Framework

mlme_rx_enable_req_tag Struct Reference

This is the MLME-RX-ENABLE.request message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 This identifies the message as MLME_RX_ENABLE_REQUEST. More...
 
uint8_t DeferPermit
 TRUE if the receiver enable can be deferred until during the next superframe if the requested time has already passed. More...
 
uint32_t RxOnDuration
 The number of symbols for which the receiver is to be enabled. More...
 
uint32_t RxOnTime
 The number of symbols from the start of the superframe before the receiver is to be enabled. More...