Microchip® Advanced Software Framework

mlme_scan_conf_tag Struct Reference

This is the MLME-SCAN.confirm message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t ChannelPage
 The channel page on which the scan was performed. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_SCAN_CONFIRM. More...
 
uint8_t ResultListSize
 The number of elements returned in the appropriate result lists. More...
 
scan_result_list_t scan_result_list [1]
 ResultListSize - The number of elements returned in the appropriate result lists. More...
 
uint8_t ScanType
 ScanType Integer 0 x 00 0 x 03 Indicates if the type of scan performed: 0 x 00 = ED scan (FFD only). More...
 
uint8_t status
 The status of the scan request. More...
 
uint32_t UnscannedChannels
 Indicates which channels given in the request were not scanned (1 = not scanned, 0 = scanned or not requested). More...