Microchip® Advanced Software Framework

mlme_scan_req_tag Struct Reference

This is the MLME-SCAN.request message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t ChannelPage
 The channel page on which to perform the scan. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_SCAN_REQUEST. More...
 
uint32_t ScanChannels
 The 5 MSBs (b27, ... More...
 
uint8_t ScanDuration
 A value used to calculate the length of time to spend scanning each channel for ED, active, and passive scans. More...
 
uint8_t ScanType
 Indicates the type of scan performed: 0 x 00 = ED scan (FFD only). More...