Microchip® Advanced Software Framework

mlme_sync_loss_ind_tag Struct Reference

This is the MLME-SYNC-LOSS.indication message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t ChannelPage
 The channel page on which the device lost synchronization or to which it was realigned. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_SYNC_LOSS_INDICATION. More...
 
uint8_t LogicalChannel
 The logical channel on which the device lost synchronization or to which it was realigned. More...
 
uint8_t LossReason
 The reason that synchronization was lost. More...
 
uint16_t PANId
 The PAN identifier with which the device lost synchronization or to which it was realigned. More...