Microchip® Advanced Software Framework

mlme_sync_req_tag Struct Reference

This is the MLME-SYNC.request message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t ChannelPage
 The channel page on which to attempt coordinator synchronization. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_SYNC_REQUEST. More...
 
uint8_t LogicalChannel
 The logical channel on which to attempt coordinator synchronization. More...
 
bool TrackBeacon
 TRUE if the MLME is to synchronize with the next beacon and attempt to track all future beacons. More...