Microchip® Advanced Software Framework

tag_qt_touch_lib_config_data_t Struct Reference

post processing configuration data that is received from the debug interface.

#include <touch_api.h>

Data Fields

uint8_t qt_di
 Sensor detect integration (DI) limit. More...
 
uint8_t qt_drift_hold_time
 Sensor drift hold time. More...
 
uint8_t qt_max_on_duration
 Sensor maximum on duration. More...
 
uint8_t qt_neg_drift_rate
 Sensor negative drift rate. More...
 
uint8_t qt_pos_drift_rate
 Sensor positive drift rate. More...
 
uint8_t qt_pos_recal_delay
 Positive recalibration delay. More...
 
recal_threshold_t qt_recal_threshold
 Sensor recalibration threshold. More...