WINC3400 IoT OTA Interface.
Copyright (c) 2017-2019 Microchip Technology Inc. and its subsidiaries.
#include "common/include/nm_common.h"
#include "driver/include/m2m_types.h"
#include "driver/source/nmdrv.h"
Typedefs | |
typedef void(* | tpfOtaNotifCb )(tstrOtaUpdateInfo *pstrOtaUpdateInfo) |
typedef void(* | tpfOtaUpdateCb )(uint8 u8OtaUpdateStatusType, uint8 u8OtaUpdateStatus) |
Functions | |
NMI_API sint8 | m2m_ota_abort (void) |
Request OTA Abort. More... | |
NMI_API sint8 | m2m_ota_init (tpfOtaUpdateCb pfOtaUpdateCb, tpfOtaNotifCb pfOtaNotifCb) |
Initialize the OTA layer. More... | |
NMI_API sint8 | m2m_ota_notif_check_for_update (void) |
Check for OTA update. More... | |
NMI_API sint8 | m2m_ota_notif_sched (uint32 u32Period) |
Schedule OTA update. More... | |
NMI_API sint8 | m2m_ota_notif_set_url (uint8 *u8Url) |
Set the OTA url. More... | |
NMI_API sint8 | m2m_ota_rollback (void) |
Request OTA Rollback image. More... | |
NMI_API sint8 | m2m_ota_start_update (unsigned char *pcDownloadUrl) |
Request OTA start update using the downloaded URL. More... | |
NMI_API sint8 | m2m_ota_switch_firmware (void) |
Switch to the upgraded Firmware. More... | |