Collection of spinners struct.
#include <gfx_mono_spinctrl.h>
Data Fields | |
bool | active_spinner |
Boolean to tell if input should be sent directly to a spinner. More... | |
struct gfx_mono_spinctrl * | collection |
Pointer to the first spinner in the collection. More... | |
struct gfx_mono_spinctrl * | collection_last |
Pointer to the last spinner in the collection. More... | |
uint8_t | current_selection |
Current spinner/button. More... | |
bool | init |
Boolean to initialize results array when starting key processing. More... | |
uint8_t | number_of_spinners |
Number of spinners in collection. More... | |
uint16_t | selection |
Return value from selected spinner. More... | |
bool gfx_mono_spinctrl_spincollection::active_spinner |
Boolean to tell if input should be sent directly to a spinner.
Referenced by gfx_mono_spinctrl_spincollection_init(), and gfx_mono_spinctrl_spincollection_process_key().
struct gfx_mono_spinctrl* gfx_mono_spinctrl_spincollection::collection |
Pointer to the first spinner in the collection.
Referenced by gfx_mono_spinctrl_spincollection_add_spinner(), gfx_mono_spinctrl_spincollection_process_key(), and gfx_mono_spinctrl_spincollection_show().
struct gfx_mono_spinctrl* gfx_mono_spinctrl_spincollection::collection_last |
Pointer to the last spinner in the collection.
Referenced by gfx_mono_spinctrl_spincollection_add_spinner(), and gfx_mono_spinctrl_spincollection_process_key().
uint8_t gfx_mono_spinctrl_spincollection::current_selection |
Current spinner/button.
Referenced by gfx_mono_spinctrl_spincollection_init(), and gfx_mono_spinctrl_spincollection_process_key().
bool gfx_mono_spinctrl_spincollection::init |
Boolean to initialize results array when starting key processing.
Referenced by gfx_mono_spinctrl_spincollection_init(), and gfx_mono_spinctrl_spincollection_process_key().
uint8_t gfx_mono_spinctrl_spincollection::number_of_spinners |
Number of spinners in collection.
Referenced by gfx_mono_spinctrl_spincollection_add_spinner(), gfx_mono_spinctrl_spincollection_init(), gfx_mono_spinctrl_spincollection_process_key(), and gfx_mono_spinctrl_spincollection_show().
uint16_t gfx_mono_spinctrl_spincollection::selection |
Return value from selected spinner.
Referenced by gfx_mono_spinctrl_spincollection_process_key().