Data Fields | |
int(* | getc )(void) |
uint32_t(* | getdata )(void *data, uint32_t length) |
uint32_t(* | getdata_xmd )(void *data, uint32_t length) |
bool(* | is_rx_ready )(void) |
int(* | putc )(int value) |
uint32_t(* | putdata )(void const *data, uint32_t length) |
uint32_t(* | putdata_xmd )(void const *data, uint32_t length) |
int(* t_monitor_if::getc)(void) |
Referenced by sam_ba_monitor_run().
Referenced by sam_ba_monitor_run().
bool(* t_monitor_if::is_rx_ready)(void) |
int(* t_monitor_if::putc)(int value) |
Referenced by sam_ba_monitor_run(), and sam_ba_putdata_term().
Referenced by sam_ba_monitor_run().