Declaration of main function used by HID keyboard unit test.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_keyboard_disable (void) |
Called by HID interface Callback running when USB Host disable keyboard interface. More... | |
bool | main_keyboard_enable (void) |
Called by HID interface Callback running when USB Host enable keyboard interface. More... | |
void | main_keyboard_led (uint8_t value) |
Called by HID interface Callback running when USB Host change keyboard leds. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_vbus_action (bool b_high) |
Called when Vbus line state change. More... | |
void main_keyboard_disable | ( | void | ) |
Called by HID interface Callback running when USB Host disable keyboard interface.
bool main_keyboard_enable | ( | void | ) |
Called by HID interface Callback running when USB Host enable keyboard interface.
true | if keyboard startup is ok |
void main_keyboard_led | ( | uint8_t | value | ) |
Called by HID interface Callback running when USB Host change keyboard leds.
References main_b_keyboard_led, and UNUSED.
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
void main_vbus_action | ( | bool | b_high | ) |
Called when Vbus line state change.