Microchip® Advanced Software Framework

common/services/usb/class/phdc/device/example/main.h File Reference

Declaration of main function used by PHDC example.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void main_phdc_disable (void)
 Called by PHDC interface Callback running when USB Host disable PHDC interface. More...
 
bool main_phdc_enable (void)
 Called by PHDC interface Callback running when USB Host enable PHDC interface. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 

void main_phdc_disable ( void  )

Called by PHDC interface Callback running when USB Host disable PHDC interface.

References ieee11073_skeleton_disable(), and main_b_phdc_enable.

bool main_phdc_enable ( void  )

Called by PHDC interface Callback running when USB Host enable PHDC interface.

Return values
trueif phdc startup is ok

References ieee11073_skeleton_enable(), and main_b_phdc_enable.

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.