Microchip® Advanced Software Framework

common/services/usb/class/phdc/device/example/ui.h File Reference

Common User Interface for PHDC application.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void ui_association (bool state)
 Calls to display the new association state. More...
 
void ui_init (void)
 Initializes the user interface. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 

void ui_association ( bool  state)

Calls to display the new association state.

Parameters
statePHDC association is done, if true

Referenced by main().

void ui_init ( void  )

Initializes the user interface.

void ui_powerdown ( void  )

Enters the user interface in power down mode.

Sets the user interface in power down mode.

void ui_process ( uint16_t  framenumber)

This process is called each 1ms It is called only if the USB interface is enabled.

Parameters
framenumberCurrent frame number
void ui_wakeup ( void  )

Exits the user interface of power down mode.