Microchip® Advanced Software Framework

etimer.h File Reference

Event timer header file.

Author
Adam Dunkels adam@.nosp@m.sics.nosp@m..se
#include "sys/timer.h"
#include "sys/process.h"

Data Structures

struct  etimer
 A timer. More...
 

Functions

 PROCESS_NAME (etimer_process)
 
Functions called from application programs
void etimer_set (struct etimer *et, clock_time_t interval)
 Set an event timer. More...
 
void etimer_reset (struct etimer *et)
 Reset an event timer with the same interval as was previously set. More...
 
void etimer_restart (struct etimer *et)
 Restart an event timer from the current point in time. More...
 
void etimer_adjust (struct etimer *et, int td)
 Adjust the expiration time for an event timer. More...
 
clock_time_t etimer_expiration_time (struct etimer *et)
 Get the expiration time for the event timer. More...
 
clock_time_t etimer_start_time (struct etimer *et)
 Get the start time for the event timer. More...
 
int etimer_expired (struct etimer *et)
 Check if an event timer has expired. More...
 
void etimer_stop (struct etimer *et)
 Stop a pending event timer. More...
 
Functions called from timer interrupts, by the system
void etimer_request_poll (void)
 Make the event timer aware that the clock has changed. More...
 
int etimer_pending (void)
 Check if there are any non-expired event timers. More...
 
clock_time_t etimer_next_expiration_time (void)
 Get next event timer expiration time. More...