Microchip® Advanced Software Framework

sys Directory Reference

Files

file  arg.c
 Argument buffer for passing arguments when starting processes.
 
file  arg.h
 
file  autostart.c
 
    Implementation of module for automatically starting and exiting a list of processes.

 
file  autostart.h
 
    Header file for module for automatically starting and exiting a list of processes.

 
file  wireless/SmartConnect_6LoWPAN/core/sys/cc.h
 Default definitions of C compiler quirk work-arounds.
 
file  compower.c
 
    Communication power accounting module

 
file  compower.h
 
    Header file for the communication power accounting module

 
file  contiki-clock.h
 
file  ctimer.c
 
    Callback timer implementation

 
file  ctimer.h
 
    Header file for the callback timer

 
file  dsc.h
 Declaration of the DSC program description structure.
 
file  energest.c
 
    Implementation of the energy estimation module

 
file  energest.h
 
    Header file for the energy estimation mechanism

 
file  etimer.c
 Event timer library implementation.
 
file  etimer.h
 Event timer header file.
 
file  lc-addrlabels.h
 Implementation of local continuations based on the "Labels as values" feature of gcc.
 
file  lc-switch.h
 Implementation of local continuations based on switch() statement.
 
file  lc.h
 Local continuations.
 
file  loader.h
 Default definitions and error values for the Contiki program loader.
 
file  log.h
 
file  mt.c
 Implementation of the archtecture agnostic parts of the preemptive multithreading library for Contiki.
 
file  mt.h
 Header file for the preemptive multitasking library for Contiki.
 
file  node-id.h
 
file  process.c
 
    Implementation of the Contiki process kernel.

 
file  process.h
 Header file for the Contiki process interface.
 
file  procinit.c
 
file  procinit.h
 
file  pt-sem.h
 Counting semaphores implemented on protothreads.
 
file  pt.h
 Protothreads implementation.
 
file  rtimer.c
 
    Implementation of the architecture-agnostic parts of the real-time timer module.

 
file  rtimer.h
 
    Header file for the real-time timer module.

 
file  stimer.c
 Timer of seconds library implementation.
 
file  stimer.h
 Second timer library header file.
 
file  subprocess.h
 
    Subprocesses for Contiki

 
file  wireless/SmartConnect_6LoWPAN/core/sys/timer.c
 Timer library implementation.
 
file  timer.h
 Timer library header file.