Implementation of local continuations based on the "Labels as values" feature of gcc.
This implementation of local continuations is based on a special feature of the GCC C compiler called "labels as values". This feature allows assigning pointers with the address of the code corresponding to a particular C label.
For more information, see the GCC documentation: http://gcc.gnu.org/onlinedocs/gcc/Labels-as-Values.html
Thanks to dividuum for finding the nice local scope label implementation.
Macros | |
#define | LC_END(s) |
#define | LC_INIT(s) s = NULL |
#define | LC_RESUME(s) |
#define | LC_SET(s) do { ({ __label__ resume; resume: (s) = &&resume; }); }while(0) |
Typedefs | |
typedef void * | lc_t |