Microchip® Advanced Software Framework

lc-switch.h File Reference

Implementation of local continuations based on switch() statement.

Author
Adam Dunkels adam@.nosp@m.sics.nosp@m..se

This implementation of local continuations uses the C switch() statement to resume execution of a function somewhere inside the function's body. The implementation is based on the fact that switch() statements are able to jump directly into the bodies of control structures such as if() or while() statements.

This implementation borrows heavily from Simon Tatham's coroutines implementation in C: http://www.chiark.greenend.org.uk/~sgtatham/coroutines.html

Macros

#define LC_END(s)   }
 
#define LC_INIT(s)   s = 0;
 
#define LC_RESUME(s)   switch(s) { case 0:
 
#define LC_SET(s)   s = __LINE__; case __LINE__:
 

Typedefs

typedef unsigned short lc_t