Second timer library header file.
#include "sys/contiki-clock.h"
Data Structures | |
struct | stimer |
A timer. More... | |
Functions | |
unsigned long | stimer_elapsed (struct stimer *t) |
The time elapsed since the timer started. More... | |
int | stimer_expired (struct stimer *t) |
Check if a timer has expired. More... | |
unsigned long | stimer_remaining (struct stimer *t) |
The time until the timer expires. More... | |
void | stimer_reset (struct stimer *t) |
Reset the timer with the same interval. More... | |
void | stimer_restart (struct stimer *t) |
Restart the timer from the current point in time. More... | |
void | stimer_set (struct stimer *t, unsigned long interval) |
Set a timer. More... | |