Microchip® Advanced Software Framework

ctimer.h File Reference

    Header file for the callback timer
Author
Adam Dunkels adam@.nosp@m.sics.nosp@m..se
#include "sys/etimer.h"

Data Structures

struct  ctimer
 

Functions

int ctimer_expired (struct ctimer *c)
 Check if a callback timer has expired. More...
 
void ctimer_init (void)
 Initialize the callback timer library. More...
 
void ctimer_reset (struct ctimer *c)
 Reset a callback timer with the same interval as was previously set. More...
 
void ctimer_restart (struct ctimer *c)
 Restart a callback timer from the current point in time. More...
 
void ctimer_set (struct ctimer *c, clock_time_t t, void(*f)(void *), void *ptr)
 Set a callback timer. More...
 
void ctimer_stop (struct ctimer *c)
 Stop a pending callback timer. More...