Microchip® Advanced Software Framework

flash.h File Reference

Functions

void flash_clear (unsigned long addr)
 
void flash_done (void)
 
void flash_init (void)
 
uint16_t flash_read (unsigned long addr)
 
void flash_setup (void)
 
void flash_write (unsigned long addr16, uint16_t data16)
 

void flash_clear ( unsigned long  addr)
void flash_done ( void  )
void flash_init ( void  )

References nvm_get_config_defaults(), and nvm_set_config().

Referenced by main().

uint16_t flash_read ( unsigned long  addr)
void flash_setup ( void  )
void flash_write ( unsigned long  addr16,
uint16_t  data16 
)