Here are listed all the functions that implement the Wifi Roaming APIs.
sint8 m2m_wifi_disable_roaming |
( |
void |
| ) |
|
Disable WiFi STA roaming.
- Precondition
- Must be called after the initialization.
- Returns
- The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
- See Also
- m2m_wifi_init
sint8 m2m_wifi_enable_roaming |
( |
uint8 |
bEnableDhcp | ) |
|
Enable WiFi STA roaming.
m2m_wifi_enable_roaming enables the firmware to trigger the roaming algorithm/steps on link loss with the current AP.
If roaming is successful, the @ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_ROAMED is sent to the host.
Additionally a @ref M2M_WIFI_REQ_DHCP_CONF message with new DHCP lease details is sent to host (only if bEnableDhcp=1).
If roaming is unsuccessful, a @ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_DISCONNECTED is sent to host.
- Parameters
-
[in] | bEnableDhcp | 0 : Disables DHCP client execution after roaming to new AP 1 : Enables DHCP client execution after roaming to new AP |
- Precondition
- Must be called after the initialization. The roaming algorithm/procedure is internal to the firmware.
- Returns
- The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
- See Also
- m2m_wifi_init
m2m_wifi_enable_roaming enables the firmware to trigger the roaming algorithm/steps on link loss with the current AP.
If roaming is successful,
the @ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_ROAMED is sent to host.
Additionally a @ref M2M_WIFI_REQ_DHCP_CONF message with new DHCP lease details is sent to host (only if bEnableDhcp=1).
If roaming is unsuccessful,
@ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_DISCONNECTED is sent to host.
- Parameters
-
[in] | bEnableDhcp | 0 : Disables DHCP client execution after roaming to new AP 1 : Enables DHCP client execution after roaming to new AP |
- Precondition
- Must be called after the initialization. The roaming algorithm/procedure is internal to the firmware.
- Returns
- The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
- See Also
- m2m_wifi_init
Referenced by main().