This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Real Time Clock functionality in Calendar operating mode, for the configuration and retrieval of the current time and date as maintained by the RTC module.
The following driver API modes are covered by this manual:
The following peripheral is used by this module:
The following devices can use this module:
The outline of this documentation is as follows:
There are no prerequisites for this module.
The RTC module in the SAM devices is a 32-bit counter, with a 10-bit programmable prescaler. Typically, the RTC clock is run continuously, including in the device's low-power sleep modes, to track the current time and date information. The RTC can be used as a source to wake up the system at a scheduled time or periodically using the alarm functions.
In this driver, the RTC is operated in Calendar mode. This allows for an easy integration of a real time clock and calendar into a user application to track the passing of time and/or perform scheduled tasks.
Whilst operating in Calendar mode, the RTC features:
Driver Feature Macro | Supported devices |
---|---|
FEATURE_RTC_PERIODIC_INT | SAM L21/L22/C20/C21/R30 |
FEATURE_RTC_PRESCALER_OFF | SAM L21/L22/C20/C21/R30 |
FEATURE_RTC_CLOCK_SELECTION | SAM L21/L22/C20/C21/R30 |
FEATURE_RTC_GENERAL_PURPOSE_REG | SAM L21/L22/R30 |
FEATURE_RTC_CONTINUOUSLY_UPDATED | SAM D20, SAM D21, SAM R21, SAM D10, SAM D11, SAM DA1, SAM HA1 |
FEATURE_RTC_TAMPER_DETECTION | SAM L22 |
The RTC has up to four independent hardware alarms that can be configured by the user application. These alarms will be triggered on match with the current clock value, and can be set up to trigger an interrupt, event, or both. The RTC can also be configured to clear the clock value on alarm match, resetting the clock to the original start time.
If the RTC is operated in clock-only mode (i.e. with calendar disabled), the RTC counter value will instead be cleared on overflow once the maximum count value has been reached:
\[ COUNT_{MAX} = 2^{32}-1 \]
When the RTC is operated with the calendar enabled and run using a nominal 1Hz input clock frequency, a register overflow will occur after 64 years.
The RTC can generate events at periodic intervals, allowing for direct peripheral actions without CPU intervention. The periodic events can be generated on the upper eight bits of the RTC prescaler, and will be generated on the rising edge transition of the specified bit. The resulting periodic frequency can be calculated by the following formula:
\[ f_{PERIODIC}=\frac{f_{ASY}}{2^{n+3}} \]
Where \(f_{ASY}\) refers to the asynchronous clock set up in the RTC module configuration. For the RTC to operate correctly in calendar mode, this frequency must be 1KHz, while the RTC's internal prescaler should be set to divide by 1024. The n parameter is the event source generator index of the RTC module. If the asynchronous clock is operated at the recommended 1KHz, the formula results in the values shown in the table below.
n | Periodic event |
---|---|
7 | 1Hz |
6 | 2Hz |
5 | 4Hz |
4 | 8Hz |
3 | 16Hz |
2 | 32Hz |
1 | 64Hz |
0 | 128Hz |
The RTC module contains Digital Frequency Correction logic to compensate for inaccurate source clock frequencies which would otherwise result in skewed time measurements. The correction scheme requires that at least two bits in the RTC module prescaler are reserved by the correction logic. As a result of this implementation, frequency correction is only available when the RTC is running from a 1Hz reference clock.
The correction procedure is implemented by subtracting or adding a single cycle from the RTC prescaler every 1024 RTC Generic Clock (GCLK) cycles. The adjustment is applied the specified number of time (maximum 127) over 976 of these periods. The corresponding correction in parts per million (PPM) will be given by:
\[ Correction(PPM) = \frac{VALUE}{999424}10^6 \]
The RTC clock will tick faster if provided with a positive correction value, and slower when given a negative correction value.
See RTC Tamper Detect.
The RTC module has a year range of 63 years from the starting year configured when the module is initialized. Dates outside the start to end year range described below will need software adjustment:
\[ [YEAR_{START}, YEAR_{START}+64] \]
The RTC is typically clocked by a specialized GCLK generator that has a smaller prescaler than the others. By default the RTC clock is on, selected to use the internal 32KHz Resistor/Capacitor (RC)-oscillator with a prescaler of 32, giving a resulting clock frequency of 1024Hz to the RTC. When the internal RTC prescaler is set to 1024, this yields an end-frequency of 1Hz for correct time keeping operations.
The implementer also has the option to set other end-frequencies. The table below lists the available RTC frequencies for each possible GCLK and RTC input prescaler options.
End-frequency | GCLK prescaler | RTC prescaler |
---|---|---|
32KHz | 1 | 1 |
1KHz | 32 | 1 |
1Hz | 32 | 1024 |
The overall RTC module clocking scheme is shown in the figure below.
The RTC clock can be selected from OSC32K, XOSC32K, or OSCULP32K. A 32KHz or 1KHz oscillator clock frequency is required. This clock must be configured and enabled in the 32KHz oscillator controller before using the RTC.
asfdoc_sam0_rtc_calendar_rtc_clk lists the available RTC clock.
RTC clock frequency | Clock source | Description |
---|---|---|
1.024kHz | ULP1K | 1.024kHz from 32KHz internal ULP oscillator |
32.768kHz | ULP32K | 32.768kHz from 32KHz internal ULP oscillator |
1.024kHz | OSC1K | 1.024kHz from 32KHz internal oscillator |
32.768kHz | OSC32K | 32.768kHz from 3KkHz internal oscillator |
1.024kHz | XOSC1K | 1.024kHz from 32KHz internal oscillator |
32.768kHz | XOSC32K | 32.768kHz from 32KHz external crystal oscillator |
For extra information, see Extra Information for RTC (CAL) Driver. This includes:
For a list of examples related to this driver, see Examples for RTC CAL Driver.
The RTC provides several selectable polarity external inputs (INn) that can be used for tamper detection. When detect, tamper inputs support the four actions:
Separate debouncers are embedded for each external input. The detection time depends on whether the debouncer operates synchronously or asynchronously, and whether majority detection is enabled or not. For details, refer to the section "Tamper Detection" of datasheet.
Modules | |
Related Project(s) | |
In this section you can find all the projects related to the SAM RTC Calendar (RTC CAL) Driver. | |
Data Structures | |
struct | rtc_calendar_alarm_time |
Alarm structure. More... | |
struct | rtc_calendar_config |
RTC configuration structure. More... | |
struct | rtc_calendar_events |
RTC Calendar event enable/disable structure. More... | |
struct | rtc_calendar_time |
Time structure. More... | |
struct | rtc_tamper_config |
RTC Tamper configuration structure. More... | |
struct | rtc_tamper_input_config |
RTC tamper input configuration structure. More... | |
Macros | |
#define | RTC_TAMPER_DETECT_EVT (1UL << 5) |
RTC tamper input event detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID0 (1UL << 0) |
RTC tamper ID0 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID1 (1UL << 1) |
RTC tamper ID1 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID2 (1UL << 2) |
RTC tamper ID2 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID3 (1UL << 3) |
RTC tamper ID3 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID4 (1UL << 4) |
RTC tamper ID4 detection bitmask. More... | |
Functions | |
void | rtc_tamper_get_stamp (struct rtc_module *const module, struct rtc_calendar_time *const time) |
Get the tamper stamp value. More... | |
#define | FEATURE_RTC_PERIODIC_INT |
Define port features set according to different device family. More... | |
#define | FEATURE_RTC_PRESCALER_OFF |
RTC prescaler is off. More... | |
#define | FEATURE_RTC_CLOCK_SELECTION |
RTC clock selection. More... | |
#define | FEATURE_RTC_GENERAL_PURPOSE_REG |
General purpose registers. More... | |
#define | FEATURE_RTC_TAMPER_DETECTION |
RTC tamper detection. More... | |
Configuration and Initialization | |
static void | rtc_calendar_get_time_defaults (struct rtc_calendar_time *const time) |
Initialize a time structure. More... | |
static void | rtc_calendar_get_config_defaults (struct rtc_calendar_config *const config) |
Gets the RTC default settings. More... | |
void | rtc_calendar_reset (struct rtc_module *const module) |
Resets the RTC module. More... | |
void | rtc_calendar_enable (struct rtc_module *const module) |
Enables the RTC module. More... | |
void | rtc_calendar_disable (struct rtc_module *const module) |
Disables the RTC module. More... | |
void | rtc_calendar_init (struct rtc_module *const module, Rtc *const hw, const struct rtc_calendar_config *const config) |
Initializes the RTC module with given configurations. More... | |
void | rtc_calendar_swap_time_mode (struct rtc_module *const module) |
Swaps between 12h and 24h clock mode. More... | |
enum status_code | rtc_calendar_frequency_correction (struct rtc_module *const module, const int8_t value) |
Calibrate for too-slow or too-fast oscillator. More... | |
Time and Alarm Management | |
uint32_t | rtc_calendar_time_to_register_value (struct rtc_module *const module, const struct rtc_calendar_time *const time) |
Convert time structure to register_value. More... | |
void | rtc_calendar_register_value_to_time (struct rtc_module *const module, const uint32_t register_value, struct rtc_calendar_time *const time) |
Convert register_value to time structure. More... | |
void | rtc_calendar_set_time (struct rtc_module *const module, const struct rtc_calendar_time *const time) |
Set the current calendar time to desired time. More... | |
void | rtc_calendar_get_time (struct rtc_module *const module, struct rtc_calendar_time *const time) |
Get the current calendar value. More... | |
enum status_code | rtc_calendar_set_alarm (struct rtc_module *const module, const struct rtc_calendar_alarm_time *const alarm, const enum rtc_calendar_alarm alarm_index) |
Set the alarm time for the specified alarm. More... | |
enum status_code | rtc_calendar_get_alarm (struct rtc_module *const module, struct rtc_calendar_alarm_time *const alarm, const enum rtc_calendar_alarm alarm_index) |
Get the current alarm time of specified alarm. More... | |
Status Flag Management | |
static bool | rtc_calendar_is_overflow (struct rtc_module *const module) |
Check if an RTC overflow has occurred. More... | |
static void | rtc_calendar_clear_overflow (struct rtc_module *const module) |
Clears the RTC overflow flag. More... | |
static bool | rtc_calendar_is_periodic_interval (struct rtc_module *const module, enum rtc_calendar_periodic_interval n) |
Check if an RTC periodic interval interrupt has occurred. More... | |
static void | rtc_calendar_clear_periodic_interval (struct rtc_module *const module, enum rtc_calendar_periodic_interval n) |
Clears the RTC periodic interval flag. More... | |
static bool | rtc_calendar_is_alarm_match (struct rtc_module *const module, const enum rtc_calendar_alarm alarm_index) |
Check the RTC alarm flag. More... | |
static enum status_code | rtc_calendar_clear_alarm_match (struct rtc_module *const module, const enum rtc_calendar_alarm alarm_index) |
Clears the RTC alarm match flag. More... | |
Event Management | |
static void | rtc_calendar_enable_events (struct rtc_module *const module, struct rtc_calendar_events *const events) |
Enables an RTC event output. More... | |
static void | rtc_calendar_disable_events (struct rtc_module *const module, struct rtc_calendar_events *const events) |
Disables an RTC event output. More... | |
RTC General Purpose Registers | |
static void | rtc_write_general_purpose_reg (struct rtc_module *const module, const uint8_t index, uint32_t value) |
Write a value into general purpose register. More... | |
static uint32_t | rtc_read_general_purpose_reg (struct rtc_module *const module, const uint8_t index) |
Read the value from general purpose register. More... | |
RTC Tamper Detection | |
static void | rtc_tamper_get_config_defaults (struct rtc_tamper_config *const config) |
Gets the RTC tamper default configurations. More... | |
enum status_code | rtc_tamper_set_config (struct rtc_module *const module, struct rtc_tamper_config *const tamper_cfg) |
static uint32_t | rtc_tamper_get_detect_flag (struct rtc_module *const module) |
Retrieves the RTC tamper detection status. More... | |
static void | rtc_tamper_clear_detect_flag (struct rtc_module *const module, const uint32_t detect_flags) |
Clears RTC tamper detection flag. More... | |
Callbacks | |
enum status_code | rtc_calendar_register_callback (struct rtc_module *const module, rtc_calendar_callback_t callback, enum rtc_calendar_callback callback_type) |
Registers callback for the specified callback type. More... | |
enum status_code | rtc_calendar_unregister_callback (struct rtc_module *const module, enum rtc_calendar_callback callback_type) |
Unregisters callback for the specified callback type. More... | |
void | rtc_calendar_enable_callback (struct rtc_module *const module, enum rtc_calendar_callback callback_type) |
Enables callback. More... | |
void | rtc_calendar_disable_callback (struct rtc_module *const module, enum rtc_calendar_callback callback_type) |
Disables callback. More... | |
#define FEATURE_RTC_CLOCK_SELECTION |
RTC clock selection.
#define FEATURE_RTC_GENERAL_PURPOSE_REG |
General purpose registers.
#define FEATURE_RTC_PERIODIC_INT |
Define port features set according to different device family.
RTC periodic interval interrupt.
#define FEATURE_RTC_PRESCALER_OFF |
RTC prescaler is off.
#define FEATURE_RTC_TAMPER_DETECTION |
RTC tamper detection.
#define RTC_TAMPER_DETECT_EVT (1UL << 5) |
RTC tamper input event detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID0 (1UL << 0) |
RTC tamper ID0 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID1 (1UL << 1) |
RTC tamper ID1 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID2 (1UL << 2) |
RTC tamper ID2 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID3 (1UL << 3) |
RTC tamper ID3 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID4 (1UL << 4) |
RTC tamper ID4 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
enum rtc_calendar_alarm |
Available mask options for alarms.
Available mask options for alarms.
Callback types.
The available callback types for the RTC calendar module.
Available periodic interval source.
RTC input clock prescaler settings.
The available input clock prescaler values for the RTC calendar module.
enum rtc_clock_sel |
Available clock source for RTC.
RTC clock source.
RTC tamper active layer frequency divider.
The available prescaler factor for the RTC clock output used during active layer protection.
RTC tamper debounce frequency divider.
The available prescaler factor for the input debouncers.
RTC tamper debounce sequential.
The available sequential for tamper debounce.
RTC tamper input action.
The available action taken by the tamper input.
enum rtc_tamper_level_sel |
|
inlinestatic |
Clears the RTC alarm match flag.
Clear the requested alarm match flag, so that future alarm matches can be determined.
[in,out] | module | Pointer to the software instance struct |
[in] | alarm_index | The index of the alarm match to clear |
STATUS_OK | If flag was cleared correctly |
STATUS_ERR_INVALID_ARG | If invalid argument(s) were provided |
References Assert, STATUS_ERR_INVALID_ARG, and STATUS_OK.
Referenced by main(), run_rtc_calendar_interrupt_test(), and run_rtc_calendar_test().
|
inlinestatic |
Clears the RTC overflow flag.
[in,out] | module | Pointer to the software instance struct |
Clears the RTC module counter overflow flag, so that new overflow conditions can be detected.
References Assert.
Referenced by run_rtc_calendar_test().
|
inlinestatic |
Clears the RTC periodic interval flag.
Clears the RTC module counter periodic interval flag, so that new periodic interval conditions can be detected.
[in,out] | module | RTC hardware module |
[in] | n | RTC periodic interval interrupt |
References Assert.
void rtc_calendar_disable | ( | struct rtc_module *const | module | ) |
Disables the RTC module.
Disables the RTC module.
[in,out] | module | Pointer to the software instance struct |
References Assert, rtc_calendar_is_syncing(), system_interrupt_disable(), and SYSTEM_INTERRUPT_MODULE_RTC.
Referenced by rtc_calendar_reset(), rtc_calendar_swap_time_mode(), run_rtc_calendar_interrupt_test(), and run_rtc_calendar_test().
void rtc_calendar_disable_callback | ( | struct rtc_module *const | module, |
enum rtc_calendar_callback | callback_type | ||
) |
Disables callback.
Disables the callback specified by the callback_type.
[in,out] | module | Pointer to the software instance struct |
[in] | callback_type | Callback type to disable |
References Assert, and RTC_CALENDAR_CALLBACK_OVERFLOW.
Referenced by run_rtc_calendar_interrupt_test().
|
inlinestatic |
Disables an RTC event output.
Disabled one or more output events from the RTC module. See rtc_calendar_events for a list of events this module supports.
[in,out] | module | Pointer to the software instance struct |
[in] | events | Struct containing flags of events to disable |
References Assert, rtc_calendar_events::generate_event_on_alarm, rtc_calendar_events::generate_event_on_overflow, rtc_calendar_events::generate_event_on_periodic, rtc_calendar_events::generate_event_on_tamper, i, and rtc_calendar_events::on_event_to_tamper.
void rtc_calendar_enable | ( | struct rtc_module *const | module | ) |
Enables the RTC module.
Enables the RTC module once it has been configured, ready for use. Most module configuration parameters cannot be altered while the module is enabled.
[in,out] | module | Pointer to the software instance struct |
References Assert, rtc_calendar_is_syncing(), system_interrupt_enable(), and SYSTEM_INTERRUPT_MODULE_RTC.
Referenced by configure_rtc_calendar(), rtc_calendar_swap_time_mode(), run_rtc_calendar_interrupt_test(), and run_rtc_calendar_test().
void rtc_calendar_enable_callback | ( | struct rtc_module *const | module, |
enum rtc_calendar_callback | callback_type | ||
) |
Enables callback.
Enables the callback specified by the callback_type.
[in,out] | module | Pointer to the software instance struct |
[in] | callback_type | Callback type to enable |
References Assert, and RTC_CALENDAR_CALLBACK_OVERFLOW.
Referenced by configure_rtc_callbacks(), and run_rtc_calendar_interrupt_test().
|
inlinestatic |
Enables an RTC event output.
Enables one or more output events from the RTC module. See rtc_calendar_events for a list of events this module supports.
[in,out] | module | Pointer to the software instance struct |
[in] | events | Struct containing flags of events to enable |
References Assert, rtc_calendar_events::generate_event_on_alarm, rtc_calendar_events::generate_event_on_overflow, rtc_calendar_events::generate_event_on_periodic, rtc_calendar_events::generate_event_on_tamper, i, and rtc_calendar_events::on_event_to_tamper.
enum status_code rtc_calendar_frequency_correction | ( | struct rtc_module *const | module, |
const int8_t | value | ||
) |
Calibrate for too-slow or too-fast oscillator.
When used, the RTC will compensate for an inaccurate oscillator. The RTC module will add or subtract cycles from the RTC prescaler to adjust the frequency in approximately 1 PPM steps. The provided correction value should be between -127 and 127, allowing for a maximum 127 PPM correction in either direction.
If no correction is needed, set value to zero.
[in,out] | module | Pointer to the software instance struct |
[in] | value | Between -127 and 127 used for the correction |
STATUS_OK | If calibration was done correctly |
STATUS_ERR_INVALID_ARG | If invalid argument(s) were provided |
References Assert, rtc_calendar_is_syncing(), STATUS_ERR_INVALID_ARG, and STATUS_OK.
enum status_code rtc_calendar_get_alarm | ( | struct rtc_module *const | module, |
struct rtc_calendar_alarm_time *const | alarm, | ||
const enum rtc_calendar_alarm | alarm_index | ||
) |
Get the current alarm time of specified alarm.
Retrieves the current alarm time for the alarm specified alarm.
[in,out] | module | Pointer to the software instance struct |
[out] | alarm | Pointer to the struct that will be filled with alarm time and mask of the specified alarm |
[in] | alarm_index | Index of alarm to get alarm time from |
STATUS_OK | If alarm was read correctly |
STATUS_ERR_INVALID_ARG | If invalid argument(s) were provided |
References Assert, rtc_calendar_alarm_time::mask, rtc_calendar_register_value_to_time(), STATUS_ERR_INVALID_ARG, STATUS_OK, and rtc_calendar_alarm_time::time.
Referenced by rtc_calendar_swap_time_mode().
|
inlinestatic |
Gets the RTC default settings.
Initializes the configuration structure to the known default values. This function should be called at the start of any RTC initiation.
The default configuration is as follows:
[out] | config | Configuration structure to be initialized to default values |
References rtc_calendar_config::alarm, Assert, rtc_calendar_config::clear_on_match, rtc_calendar_config::clock_24h, i, rtc_calendar_alarm_time::mask, rtc_calendar_config::prescaler, RTC_CALENDAR_ALARM_MASK_YEAR, rtc_calendar_get_time_defaults(), RTC_CALENDAR_PRESCALER_DIV_1024, rtc_calendar_alarm_time::time, and rtc_calendar_config::year_init_value.
Referenced by configure_rtc_calendar(), and run_rtc_calendar_test().
void rtc_calendar_get_time | ( | struct rtc_module *const | module, |
struct rtc_calendar_time *const | time | ||
) |
Get the current calendar value.
Retrieves the current time of the calendar.
[in,out] | module | Pointer to the software instance struct |
[out] | time | Pointer to value that will be filled with current time |
References Assert, rtc_calendar_is_syncing(), and rtc_calendar_register_value_to_time().
Referenced by get_fattime(), and rtc_calendar_swap_time_mode().
|
inlinestatic |
Initialize a time
structure.
This will initialize a given time structure to the time 00:00:00 (hh:mm:ss) and date 2000-01-01 (YYYY-MM-DD).
[out] | time | Time structure to initialize |
References rtc_calendar_time::day, rtc_calendar_time::hour, rtc_calendar_time::minute, rtc_calendar_time::month, rtc_calendar_time::pm, rtc_calendar_time::second, and rtc_calendar_time::year.
Referenced by main(), rtc_calendar_get_config_defaults(), and run_rtc_calendar_test().
void rtc_calendar_init | ( | struct rtc_module *const | module, |
Rtc *const | hw, | ||
const struct rtc_calendar_config *const | config | ||
) |
Initializes the RTC module with given configurations.
Initializes the module, setting up all given configurations to provide the desired functionality of the RTC.
[out] | module | Pointer to the software instance struct |
[in] | hw | Pointer to hardware instance |
[in] | config | Pointer to the configuration structure |
References _rtc_calendar_set_config(), _rtc_instance, Assert, rtc_calendar_config::clock_24h, GCLK_GENERATOR_2, rtc_calendar_reset(), system_gclk_chan_config::source_generator, system_apb_clock_set_mask(), SYSTEM_CLOCK_APB_APBA, system_gclk_chan_enable(), system_gclk_chan_get_config_defaults(), system_gclk_chan_set_config(), and rtc_calendar_config::year_init_value.
Referenced by configure_rtc_calendar(), and run_rtc_calendar_test().
|
inlinestatic |
Check the RTC alarm flag.
Check if the specified alarm flag is set. The flag is set when there is a compare match between the alarm value and the clock.
[in,out] | module | Pointer to the software instance struct |
[in] | alarm_index | Index of the alarm to check |
true | If the specified alarm has matched the current time |
false | If the specified alarm has not matched the current time |
References Assert.
Referenced by main(), and run_rtc_calendar_test().
|
inlinestatic |
Check if an RTC overflow has occurred.
Checks the overflow flag in the RTC. The flag is set when there is an overflow in the clock.
[in,out] | module | Pointer to the software instance struct |
true | If the RTC count value has overflowed |
false | If the RTC count value has not overflowed |
References Assert.
Referenced by run_rtc_calendar_test().
|
inlinestatic |
Check if an RTC periodic interval interrupt has occurred.
Checks the periodic interval flag in the RTC.
[in,out] | module | RTC hardware module |
[in] | n | RTC periodic interval interrupt |
true | RTC periodic interval interrupt occur |
false | RTC periodic interval interrupt doesn't occur |
References Assert.
enum status_code rtc_calendar_register_callback | ( | struct rtc_module *const | module, |
rtc_calendar_callback_t | callback, | ||
enum rtc_calendar_callback | callback_type | ||
) |
Registers callback for the specified callback type.
Associates the given callback function with the specified callback type. To enable the callback, the rtc_calendar_enable_callback function must be used.
[in,out] | module | Pointer to the software instance struct |
[in] | callback | Pointer to the function desired for the specified callback |
[in] | callback_type | Callback type to register |
STATUS_OK | Registering was done successfully |
STATUS_ERR_INVALID_ARG | If trying to register, a callback is not available |
References callback, RTC_CALENDAR_CALLBACK_OVERFLOW, status, STATUS_ERR_INVALID_ARG, and STATUS_OK.
Referenced by configure_rtc_callbacks(), and run_rtc_calendar_interrupt_test().
void rtc_calendar_register_value_to_time | ( | struct rtc_module *const | module, |
const uint32_t | register_value, | ||
struct rtc_calendar_time *const | time | ||
) |
Convert register_value to time structure.
Retrieves the time structure convert by register_value.
[in,out] | module | Pointer to the software instance struct |
[in] | register_value | The value stored in register |
[out] | time | Pointer to the time structure |
References rtc_calendar_time::day, rtc_calendar_time::hour, rtc_calendar_time::minute, rtc_calendar_time::month, rtc_calendar_time::pm, rtc_calendar_time::second, and rtc_calendar_time::year.
Referenced by rtc_calendar_get_alarm(), and rtc_calendar_get_time().
void rtc_calendar_reset | ( | struct rtc_module *const | module | ) |
Resets the RTC module.
Resets the RTC module to hardware defaults.
[in,out] | module | Pointer to the software instance struct |
References Assert, rtc_calendar_disable(), and rtc_calendar_is_syncing().
Referenced by rtc_calendar_init().
enum status_code rtc_calendar_set_alarm | ( | struct rtc_module *const | module, |
const struct rtc_calendar_alarm_time *const | alarm, | ||
const enum rtc_calendar_alarm | alarm_index | ||
) |
Set the alarm time for the specified alarm.
Sets the time and mask specified to the requested alarm.
[in,out] | module | Pointer to the software instance struct |
[in] | alarm | The alarm struct to set the alarm with |
[in] | alarm_index | The index of the alarm to set |
STATUS_OK | If alarm was set correctly |
STATUS_ERR_INVALID_ARG | If invalid argument(s) were provided |
References Assert, rtc_calendar_alarm_time::mask, rtc_calendar_is_syncing(), rtc_calendar_time_to_register_value(), STATUS_ERR_INVALID_ARG, STATUS_OK, and rtc_calendar_alarm_time::time.
Referenced by _rtc_calendar_set_config(), rtc_calendar_swap_time_mode(), rtc_match_callback(), run_rtc_calendar_interrupt_test(), and run_rtc_calendar_test().
void rtc_calendar_set_time | ( | struct rtc_module *const | module, |
const struct rtc_calendar_time *const | time | ||
) |
Set the current calendar time to desired time.
Sets the time provided to the calendar.
[in,out] | module | Pointer to the software instance struct |
[in] | time | The time to set in the calendar |
References Assert, rtc_calendar_is_syncing(), and rtc_calendar_time_to_register_value().
Referenced by main(), rtc_calendar_swap_time_mode(), run_rtc_calendar_interrupt_test(), and run_rtc_calendar_test().
void rtc_calendar_swap_time_mode | ( | struct rtc_module *const | module | ) |
Swaps between 12h and 24h clock mode.
Swaps the current RTC time mode:
[in,out] | module | Pointer to the software instance struct |
References Assert, rtc_calendar_time::hour, i, rtc_calendar_time::pm, rtc_calendar_disable(), rtc_calendar_enable(), rtc_calendar_get_alarm(), rtc_calendar_get_time(), rtc_calendar_set_alarm(), rtc_calendar_set_time(), and rtc_calendar_alarm_time::time.
Referenced by main().
uint32_t rtc_calendar_time_to_register_value | ( | struct rtc_module *const | module, |
const struct rtc_calendar_time *const | time | ||
) |
Convert time structure to register_value.
Retrieves register_value convert by the time structure.
[in,out] | module | Pointer to the software instance struct |
[in] | time | Pointer to the time structure |
References rtc_calendar_time::day, rtc_calendar_time::hour, rtc_calendar_time::minute, rtc_calendar_time::month, rtc_calendar_time::pm, rtc_calendar_time::second, and rtc_calendar_time::year.
Referenced by rtc_calendar_set_alarm(), and rtc_calendar_set_time().
enum status_code rtc_calendar_unregister_callback | ( | struct rtc_module *const | module, |
enum rtc_calendar_callback | callback_type | ||
) |
Unregisters callback for the specified callback type.
When called, the currently registered callback for the given callback type will be removed.
[in,out] | module | Pointer to the software instance struct |
[in] | callback_type | Specifies the callback type to unregister |
STATUS_OK | Unregistering was done successfully |
STATUS_ERR_INVALID_ARG | If trying to unregister, a callback is not available |
References NULL, RTC_CALENDAR_CALLBACK_OVERFLOW, status, STATUS_ERR_INVALID_ARG, and STATUS_OK.
Referenced by run_rtc_calendar_interrupt_test().
|
inlinestatic |
Read the value from general purpose register.
[in] | module | Pointer to the software instance struct |
[in] | index | General purpose register index (0..3) |
References Assert.
|
inlinestatic |
Clears RTC tamper detection flag.
Clears the given detection flag of the module.
[in] | module | Pointer to the TC software instance struct |
[in] | detect_flags | Bitmask of detection flags |
References Assert, RTC_TAMPER_DETECT_EVT, RTC_TAMPER_DETECT_ID0, RTC_TAMPER_DETECT_ID1, RTC_TAMPER_DETECT_ID2, RTC_TAMPER_DETECT_ID3, and RTC_TAMPER_DETECT_ID4.
|
inlinestatic |
Gets the RTC tamper default configurations.
Initializes the configuration structure to default values.
The default configuration is as follows:
[out] | config | Configuration structure to be initialized to default values. |
References rtc_tamper_input_config::action, rtc_tamper_config::actl_freq_div, Assert, rtc_tamper_config::bkup_reset_on_tamper, rtc_tamper_config::deb_freq_div, rtc_tamper_config::deb_seq, rtc_tamper_input_config::debounce_enable, rtc_tamper_config::dma_tamper_enable, rtc_tamper_config::gp0_enable, rtc_tamper_config::gp_reset_on_tamper, id, rtc_tamper_config::in_cfg, rtc_tamper_input_config::level, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_8, RTC_TAMPER_DEBOUNCE_FREQ_DIV_8, RTC_TAMPER_DEBOUNCE_SYNC, RTC_TAMPER_INPUT_ACTION_OFF, and RTC_TAMPER_LEVEL_FALLING.
|
inlinestatic |
Retrieves the RTC tamper detection status.
Retrieves the detection status of each input pin and the input event.
[in] | module | Pointer to the RTC software instance struct |
RTC_TAMPER_DETECT_ID0 | Tamper condition on IN0 has been detected |
RTC_TAMPER_DETECT_ID1 | Tamper condition on IN1 has been detected |
RTC_TAMPER_DETECT_ID2 | Tamper condition on IN2 has been detected |
RTC_TAMPER_DETECT_ID3 | Tamper condition on IN3 has been detected |
RTC_TAMPER_DETECT_ID4 | Tamper condition on IN4 has been detected |
RTC_TAMPER_DETECT_EVT | Tamper input event has been detected |
References Assert, RTC_TAMPER_DETECT_EVT, RTC_TAMPER_DETECT_ID0, RTC_TAMPER_DETECT_ID1, RTC_TAMPER_DETECT_ID2, RTC_TAMPER_DETECT_ID3, and RTC_TAMPER_DETECT_ID4.
void rtc_tamper_get_stamp | ( | struct rtc_module *const | module, |
struct rtc_calendar_time *const | time | ||
) |
Get the tamper stamp value.
[in,out] | module | Pointer to the software instance struct |
[out] | time | Pointer to value that filled with tamper stamp time |
enum status_code rtc_tamper_set_config | ( | struct rtc_module *const | module, |
struct rtc_tamper_config *const | tamper_cfg | ||
) |
|
inlinestatic |
Write a value into general purpose register.
[in] | module | Pointer to the software instance struct |
[in] | n | General purpose type |
[in] | index | General purpose register index (0..3) |
References Assert.