Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages

Handles all User interface related functions such as Button, Print,LED events.

Data Structures

struct  print_event_msg_t
 Print event message stucture to organize the prints. More...
 

Macros

#define COUNT_FOR_VALID_KEY_PRESS   (20)
 This defines the count to detect a valid key press. More...
 
#define LED_ON_DURAION_MICRO_SEC   (100000)
 This defines the LED on duration. More...
 

Functions

bool button_pressed (void)
 Determine if button is pressed. More...
 

Variables

void(* print_event_msg_t::additional_print_func )(void)
 
const char * print_event_msg_t::item_desc
 
print_event_msg_t print_event_table [NUM_MAX_PRINT_EVENTS]
 This table holds the Messages to be printed on the UART Terminal at each event. More...
 

LED EVENTS

enum  led_event_t {
  LED_EVENT_TX_FRAME,
  LED_EVENT_RX_FRAME,
  LED_EVENT_POWER_ON,
  LED_EVENT_START_PEER_SEARCH,
  LED_EVENT_PEER_SEARCH_DONE,
  LED_EVENT_ALL_ON,
  LED_EVENT_ALL_OFF
}
 

PRINT EVENTS

enum  print_event_t {
  PRINT_KEY_PRESS_WHILE_POWER_ON_CONFIG_MODE,
  PRINT_KEY_PRESS_PEER_SEARCH_INITIATOR,
  PRINT_UART_CHAR_PEER_SEARCH_INITIATOR,
  PRINT_KEY_PRESS_PEER_SEARCH_RECEPTOR,
  PRINT_UART_CHAR_PEER_SEARCH_RECEPTOR,
  PRINT_PEER_SEARCH_RECEPTOR_BAD_FRAME,
  PRINT_PEER_SEARCH_INITATED,
  PRINT_PEER_SEARCH_IN_PROGRESS,
  PRINT_PEER_SEARCH_SUCCESS,
  PRINT_PEER_SEARCH_FAILED,
  PRINT_PEER_SEARCH_ABORTED,
  PRINT_PEER_SEARCH_ABORTABLE,
  PRINT_PEER_FOUND_PER_INITIATOR,
  PRINT_PEER_FOUND_PER_RECEPTOR,
  PRINT_SINGLE_NODE_TESTS,
  PRINT_RANGE_MEASURE_TX_START,
  PRINT_RANGE_MEASURE_TX_STOP,
  PRINT_RANGE_MEASURE_STATSTICS,
  NUM_MAX_PRINT_EVENTS
}
 
volatile bool button_pressed = false
 Determine if button is pressed. More...
 
bool app_debounce_button (void)
 Button debounce routine. More...
 
void app_led_event (led_event_t ev)
 Turns LEDs on / off to indicate specific events. More...
 
void print_event (print_event_t ev)
 Print various messages from the table as per the event notified. More...
 
void app_print_statistics (void)
 Print the statistics for Range Measurement on the UART Terminal. More...
 

#define COUNT_FOR_VALID_KEY_PRESS   (20)

This defines the count to detect a valid key press.

Referenced by app_debounce_button().

#define LED_ON_DURAION_MICRO_SEC   (100000)

This defines the LED on duration.

Referenced by app_led_event().

Enumerator
LED_EVENT_TX_FRAME 
LED_EVENT_RX_FRAME 
LED_EVENT_POWER_ON 
LED_EVENT_START_PEER_SEARCH 
LED_EVENT_PEER_SEARCH_DONE 
LED_EVENT_ALL_ON 
LED_EVENT_ALL_OFF 
Enumerator
PRINT_KEY_PRESS_WHILE_POWER_ON_CONFIG_MODE 
PRINT_KEY_PRESS_PEER_SEARCH_INITIATOR 
PRINT_UART_CHAR_PEER_SEARCH_INITIATOR 
PRINT_KEY_PRESS_PEER_SEARCH_RECEPTOR 
PRINT_UART_CHAR_PEER_SEARCH_RECEPTOR 
PRINT_PEER_SEARCH_RECEPTOR_BAD_FRAME 
PRINT_PEER_SEARCH_INITATED 
PRINT_PEER_SEARCH_IN_PROGRESS 
PRINT_PEER_SEARCH_SUCCESS 
PRINT_PEER_SEARCH_FAILED 
PRINT_PEER_SEARCH_ABORTED 
PRINT_PEER_SEARCH_ABORTABLE 
PRINT_PEER_FOUND_PER_INITIATOR 
PRINT_PEER_FOUND_PER_RECEPTOR 
PRINT_SINGLE_NODE_TESTS 
PRINT_RANGE_MEASURE_TX_START 
PRINT_RANGE_MEASURE_TX_STOP 
PRINT_RANGE_MEASURE_STATSTICS 
NUM_MAX_PRINT_EVENTS 

bool app_debounce_button ( void  )

Button debounce routine.

Helper function for debouncing the transmit button.

Returns
ret 1 if a button event is detected, 0 otherwise.

References button_pressed, COUNT_FOR_VALID_KEY_PRESS, and ret.

Referenced by per_mode_receptor_task(), range_test_tx_off_task(), range_test_tx_on_task(), and wait_for_event_task().

void app_print_statistics ( void  )

Print the statistics for Range Measurement on the UART Terminal.

References num_of_frames_rec, num_of_frames_send, and printf.

bool button_pressed ( void  )

Determine if button is pressed.

Returns
true if button is pressed, else false

References ioport_get_pin_level(), and port_pin_get_input_level().

void(* print_event_msg_t::additional_print_func)(void)

Referenced by print_event().

bool button_pressed = false

Determine if button is pressed.

Returns
true if button is pressed, else false

Referenced by app_debounce_button(), button_cb(), configuration_mode_selection(), htp_temperature_send(), htpt_custom_event(), pxp_monitor_app_button_event(), and tip_app_custom_event().

const char* print_event_msg_t::item_desc

This table holds the Messages to be printed on the UART Terminal at each event.