PubNub Example.
Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.
#include "socket/include/socket.h"
Data Structures | |
struct | pubnub |
Macros | |
#define | PUBNUB_BUF_MAXLEN (256) |
#define | PUBNUB_CTX_MAX (2) |
#define | PUBNUB_ORIGIN "pubsub.pubnub.com" |
#define | PUBNUB_ORIGIN_PORT (80) |
#define | PUBNUB_PRINTF(x) |
Use PUBNUB_ENABLE_DEBUG macro to enable/disable PubNub debug. More... | |
#define | PUBNUB_REPLY_MAXLEN (512) |
#define | PUBNUB_REQUEST "GET %s HTTP/1.1\r\nHost: %s\r\nUser-Agent: PubNub-WINC1500\r\nConnection: Keep-Alive\r\n\r\n" |
Typedefs | |
typedef struct pubnub | pubnub_t |
Functions | |
void | handle_dns_found (const char *name, uint32_t hostip) |
void | handle_tcpip (SOCKET sock, uint8_t u8Msg, void *pvMsg) |
char const * | pubnub_get (pubnub_t *pb) |
pubnub_t * | pubnub_get_ctx (uint8_t index) |
Return a context for the given index. More... | |
void | pubnub_init (pubnub_t *pb, const char *publish_key, const char *subscribe_key) |
Initialize the PubNub Client API. More... | |
bool | pubnub_publish (pubnub_t *pb, const char *channel, const char *message) |
bool | pubnub_subscribe (pubnub_t *pb, const char *channel) |
#define PUBNUB_BUF_MAXLEN (256) |
Referenced by handle_transaction().
#define PUBNUB_CTX_MAX (2) |
Referenced by handle_dns_found(), handle_tcpip_recv(), pubnub_find_ctx(), pubnub_get_ctx(), and valid_ctx_prt().
#define PUBNUB_ORIGIN "pubsub.pubnub.com" |
Referenced by handle_dns_found(), handle_start_connect(), and handle_transaction().
#define PUBNUB_ORIGIN_PORT (80) |
Referenced by handle_start_connect().
#define PUBNUB_PRINTF | ( | x | ) |
Use PUBNUB_ENABLE_DEBUG macro to enable/disable PubNub debug.
Referenced by handle_tcpip(), handle_tcpip_connect(), handle_tcpip_recv(), handle_transaction(), and pubnub_publish().
#define PUBNUB_REPLY_MAXLEN (512) |
Referenced by pubnub_subscribe().
#define PUBNUB_REQUEST "GET %s HTTP/1.1\r\nHost: %s\r\nUser-Agent: PubNub-WINC1500\r\nConnection: Keep-Alive\r\n\r\n" |
Referenced by handle_transaction().
enum pubnub_res |
Enumerator | |
---|---|
PNR_OK |
Success. Transaction finished successfully. |
PNR_TIMEOUT |
Time out before the request has completed. |
PNR_IO_ERROR |
Communication error (network or HTTP response format). |
PNR_HTTP_ERROR |
HTTP error. |
PNR_FORMAT_ERROR |
Unexpected input in received JSON. |
PNR_CANCELLED |
Request cancelled by user. |
PNR_STARTED |
Transaction started. Await the outcome via process message. |
PNR_IN_PROGRESS |
Transaction (already) ongoing. Can't start a new transaction. |
PNR_RX_BUFF_NOT_EMPTY |
Receive buffer (from previous transaction) not read, new subscription not allowed. |
PNR_TX_BUFF_TOO_SMALL |
The buffer is to small. Increase PUBNUB_BUF_MAXLEN. |
PNR_OK |
Success. Transaction finished successfully. |
PNR_TIMEOUT |
Time out before the request has completed. |
PNR_IO_ERROR |
Communication error (network or HTTP response format). |
PNR_HTTP_ERROR |
HTTP error. |
PNR_FORMAT_ERROR |
Unexpected input in received JSON. |
PNR_CANCELLED |
Request cancelled by user. |
PNR_STARTED |
Transaction started. Await the outcome via process message. |
PNR_IN_PROGRESS |
Transaction (already) ongoing. Can't start a new transaction. |
PNR_RX_BUFF_NOT_EMPTY |
Receive buffer (from previous transaction) not read, new subscription not allowed. |
PNR_TX_BUFF_TOO_SMALL |
The buffer is to small. Increase PUBNUB_BUF_MAXLEN. |
enum pubnub_state |
enum pubnub_trans |
Enumerator | |
---|---|
PBTT_NONE |
No transaction at all. |
PBTT_SUBSCRIBE |
Subscribe transaction. |
PBTT_PUBLISH |
Publish transaction. |
PBTT_LEAVE |
Leave (channel(s)) transaction. |
PBTT_NONE |
No transaction at all. |
PBTT_SUBSCRIBE |
Subscribe transaction. |
PBTT_PUBLISH |
Publish transaction. |
PBTT_LEAVE |
Leave (channel(s)) transaction. |
void handle_dns_found | ( | const char * | name, |
uint32_t | hostip | ||
) |
void handle_tcpip | ( | SOCKET | sock, |
uint8_t | u8Msg, | ||
void * | pvMsg | ||
) |
char const* pubnub_get | ( | pubnub_t * | pb | ) |
pubnub_t* pubnub_get_ctx | ( | uint8_t | index | ) |
Return a context for the given index.
Contexts are statically allocated by the PubNub library and this is the only to get a pointer to one of them.
void pubnub_init | ( | pubnub_t * | pb, |
const char * | publish_key, | ||
const char * | subscribe_key | ||
) |
Initialize the PubNub Client API.