Microchip® Advanced Software Framework

next_dst.h File Reference

Next DST Change Service Application declarations.

Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.

#include "ble_manager.h"

Data Structures

struct  gatt_dst_handler
 

Macros

#define DST_INVALID_CHAR_HANDLE   (0)
 
#define DST_READ_LENGTH   (8)
 
#define DST_READ_OFFSET   (0)
 

Typedefs

typedef struct gatt_dst_handler gatt_dst_handler_t
 

Functions

at_ble_status_t tis_dst_change_read (at_ble_handle_t conn_handle, at_ble_handle_t char_handle)
 Send the Read request to the current time characteristic Read value will be reported via AT_BLE_CHARACTERISTIC_READ_RESPONSE event. More...
 
int8_t tis_dst_change_read_response (at_ble_characteristic_read_response_t *read_resp, gatt_dst_handler_t *dst_handler)
 Read response handler for read response. More...
 

#define DST_INVALID_CHAR_HANDLE   (0)

Referenced by tis_dst_change_read().

#define DST_READ_LENGTH   (8)

Referenced by tis_dst_change_read().

#define DST_READ_OFFSET   (0)

Referenced by tis_dst_change_read().

at_ble_status_t tis_dst_change_read ( at_ble_handle_t  conn_handle,
at_ble_handle_t  char_handle 
)

Send the Read request to the current time characteristic Read value will be reported via AT_BLE_CHARACTERISTIC_READ_RESPONSE event.

Parameters
[in]conn_handlehandle of the connection
[in]char_handlehandle of the characteristic
Returns
AT_BLE_SUCCESS operation completed successfully
AT_BLE_INVALID_PARAM Invalid arguments.
AT_BLE_FAILURE Generic error.

Send the Read request to the current time characteristic Read value will be reported via AT_BLE_CHARACTERISTIC_READ_RESPONSE event.

References at_ble_characteristic_read(), AT_BLE_INVALID_STATE, DST_INVALID_CHAR_HANDLE, DST_READ_LENGTH, and DST_READ_OFFSET.

Referenced by app_read_response_cb().

int8_t tis_dst_change_read_response ( at_ble_characteristic_read_response_t read_resp,
gatt_dst_handler_t dst_handler 
)

Read response handler for read response.

Parameters
[in]read_valueread response data available form at_ble_characteristic_read_response_t
Returns
Current time value.
LLS_READ_RESP_INVALID if value are other than alert levels

Read response handler for read response.

References AT_BLE_SUCCESS, at_ble_characteristic_read_response_t::char_handle, at_ble_characteristic_read_response_t::char_value, DBG_LOG, DBG_LOG_CONT, gatt_dst_handler::dst_char_handle, and at_ble_characteristic_read_response_t::status.

Referenced by time_info_characteristic_read_response(), and time_info_notification_handler().