Header file for the Rime buffer (packetbuf) management
- Author
- Adam Dunkels adam@.nosp@m.sics.nosp@m..se
|
const linkaddr_t * | packetbuf_addr (uint8_t type) |
|
packetbuf_attr_t | packetbuf_attr (uint8_t type) |
|
void | packetbuf_attr_clear (void) |
|
void | packetbuf_attr_copyfrom (struct packetbuf_attr *attrs, struct packetbuf_addr *addrs) |
|
void | packetbuf_attr_copyto (struct packetbuf_attr *attrs, struct packetbuf_addr *addrs) |
|
void | packetbuf_clear (void) |
| Clear and reset the packetbuf. More...
|
|
void | packetbuf_clear_hdr (void) |
| Clear and reset the header of the packetbuf. More...
|
|
void | packetbuf_compact (void) |
| Compact the packetbuf. More...
|
|
int | packetbuf_copyfrom (const void *from, uint16_t len) |
| Copy from external data into the packetbuf. More...
|
|
int | packetbuf_copyto (void *to) |
| Copy the entire packetbuf to an external buffer. More...
|
|
int | packetbuf_copyto_hdr (uint8_t *to) |
| Copy the header portion of the packetbuf to an external buffer. More...
|
|
uint16_t | packetbuf_datalen (void) |
| Get the length of the data in the packetbuf. More...
|
|
void * | packetbuf_dataptr (void) |
| Get a pointer to the data in the packetbuf. More...
|
|
void | packetbuf_hdr_remove (int size) |
|
int | packetbuf_hdralloc (int size) |
| Extend the header of the packetbuf, for outbound packets. More...
|
|
uint8_t | packetbuf_hdrlen (void) |
| Get the length of the header in the packetbuf, for outbound packets. More...
|
|
void * | packetbuf_hdrptr (void) |
| Get a pointer to the header in the packetbuf, for outbound packets. More...
|
|
int | packetbuf_hdrreduce (int size) |
| Reduce the header in the packetbuf, for incoming packets. More...
|
|
int | packetbuf_is_reference (void) |
| Check if the packetbuf references external data. More...
|
|
void | packetbuf_reference (void *ptr, uint16_t len) |
| Point the packetbuf to external data. More...
|
|
void * | packetbuf_reference_ptr (void) |
| Get a pointer to external data referenced by the packetbuf. More...
|
|
int | packetbuf_set_addr (uint8_t type, const linkaddr_t *addr) |
|
int | packetbuf_set_attr (uint8_t type, const packetbuf_attr_t val) |
|
void | packetbuf_set_datalen (uint16_t len) |
| Set the length of the data in the packetbuf. More...
|
|
uint16_t | packetbuf_totlen (void) |
| Get the total length of the header and data in the packetbuf. More...
|
|