Microchip® Advanced Software Framework

sam0/applications/samba_bootloader/main.h File Reference

Main functions.

Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.

#include "usb_protocol_cdc.h"

Functions

void main_cdc_disable (uint8_t port)
 Closes the communication port This is called by CDC interface when USB Host disable it. More...
 
bool main_cdc_enable (uint8_t port)
 Opens the communication port This is called by CDC interface when USB Host enable it. More...
 
void main_cdc_rx_notify (uint8_t port)
 Called by CDC interface Callback running when CDC device have received data. More...
 
void main_cdc_set_coding (uint8_t port, usb_cdc_line_coding_t *cfg)
 Configures communication line. More...
 
void main_cdc_set_dtr (uint8_t port, bool b_enable)
 Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port. More...
 
void main_remotewakeup_lpm_disable (void)
 Called by UDC when USB Host request to disable LPM remote wakeup. More...
 
void main_remotewakeup_lpm_enable (void)
 Called by UDC when USB Host request to enable LPM remote wakeup. More...
 
void main_suspend_lpm_action (void)
 Enters the application in low power mode Callback called when USB host sets LPM suspend state. More...
 

void main_cdc_disable ( uint8_t  port)

Closes the communication port This is called by CDC interface when USB Host disable it.

References b_com_port_opened, i2c_master_disable(), i2c_master_instance, main_b_cdc_enable, and uart_close().

bool main_cdc_enable ( uint8_t  port)

Opens the communication port This is called by CDC interface when USB Host enable it.

Return values
trueif cdc startup is successfully done

Called by CDC interface Callback running when USB Host enable CDC interface.

Return values
trueif cdc startup is successfully done

References configure_i2c_master(), main_b_cdc_enable, and uart_open().

void main_cdc_rx_notify ( uint8_t  port)

Called by CDC interface Callback running when CDC device have received data.

void main_cdc_set_coding ( uint8_t  port,
usb_cdc_line_coding_t cfg 
)

Configures communication line.

Parameters
cfgline configuration
void main_cdc_set_dtr ( uint8_t  port,
bool  b_enable 
)

Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port.

References b_com_port_opened, ui_com_close(), and ui_com_open().

void main_remotewakeup_lpm_disable ( void  )

Called by UDC when USB Host request to disable LPM remote wakeup.

References ui_wakeup_disable().

void main_remotewakeup_lpm_enable ( void  )

Called by UDC when USB Host request to enable LPM remote wakeup.

References ui_wakeup_enable().

void main_suspend_lpm_action ( void  )

Enters the application in low power mode Callback called when USB host sets LPM suspend state.

References ui_powerdown().