SLIP header file.
#include "uip.h"
Functions | |
uint8_t | slipdev_char_poll (uint8_t *c) |
Poll the serial device for a character. More... | |
void | slipdev_char_put (uint8_t c) |
Put a character on the serial device. More... | |
void | slipdev_init (void) |
Initialize the SLIP module. More... | |
uint16_t | slipdev_poll (void) |
Poll the SLIP device for an available packet. More... | |
uint8_t | slipdev_send (void) |
Send the packet in the uip_buf and uip_appdata buffers using the SLIP protocol. More... | |