Microchip® Advanced Software Framework

at_ble_char_list Struct Reference

Encapsulation for a characteristic and its length.

#include <at_ble_api.h>

Data Fields

uint16_t att_handle
 Characteristic handle. More...
 
uint16_t att_len
 Characteristic length : must be the real length of the Characteristic every requested handle shall be delivered as one indication at_ble_characteristic_read_response_t if Length of handle 1 is larger than the real length, the handle value will contain his length + length from the other requested handles. More...
 

uint16_t at_ble_char_list::att_handle

Characteristic handle.

uint16_t at_ble_char_list::att_len

Characteristic length : must be the real length of the Characteristic every requested handle shall be delivered as one indication at_ble_characteristic_read_response_t if Length of handle 1 is larger than the real length, the handle value will contain his length + length from the other requested handles.