data type of DMT status and report, "number_of_packets" will be used only in case of receiving the event AT_BLE_LE_PACKET_REPORT after calling the API
#include <at_ble_api.h>
Data Fields | |
uint16_t | number_of_packets |
Number of packets received (Read this variable only after calling at_ble_dtm_stop_test api with Event AT_BLE_LE_PACKET_REPORT) More... | |
uint16_t | op_code |
op-code for the current operation refer to dtm_op_codes More... | |
uint8_t | status |
status of the current command (events AT_BLE_LE_PACKET_REPORT and AT_BLE_LE_TEST_STATUS ) More... | |
uint16_t at_ble_dtm_t::number_of_packets |
Number of packets received (Read this variable only after calling at_ble_dtm_stop_test api with Event AT_BLE_LE_PACKET_REPORT)
uint16_t at_ble_dtm_t::op_code |
op-code for the current operation refer to dtm_op_codes
uint8_t at_ble_dtm_t::status |
status of the current command (events AT_BLE_LE_PACKET_REPORT and AT_BLE_LE_TEST_STATUS )