#include <at_ble_api.h>
Data Fields | |
at_ble_handle_t | handle |
user descriptor handle More... | |
uint16_t | len |
the user friendly description length, this value will be stored in the relevant descriptor, if no user description is desired set to 0 More... | |
at_ble_attr_permissions_t | permissions |
user descriptor permissions More... | |
uint8_t * | user_description |
a user friendly description, this value will be stored in the relevant descriptor, if no user description is desired set to NULL More... | |
at_ble_handle_t at_ble_user_desc_t::handle |
user descriptor handle
Referenced by hid_serv_init().
uint16_t at_ble_user_desc_t::len |
the user friendly description length, this value will be stored in the relevant descriptor, if no user description is desired set to 0
Referenced by hid_serv_init().
at_ble_attr_permissions_t at_ble_user_desc_t::permissions |
user descriptor permissions
Referenced by hid_serv_init().
uint8_t* at_ble_user_desc_t::user_description |
a user friendly description, this value will be stored in the relevant descriptor, if no user description is desired set to NULL
Referenced by hid_serv_init().