Microchip® Advanced Software Framework

broadcast_callbacks Struct Reference

Callback structure for broadcast.

#include <broadcast.h>

Data Fields

void(* recv )(struct broadcast_conn *ptr, const linkaddr_t *sender)
 Called when a packet has been received by the broadcast module. More...
 
void(* sent )(struct broadcast_conn *ptr, int status, int num_tx)
 

void(* broadcast_callbacks::recv)(struct broadcast_conn *ptr, const linkaddr_t *sender)

Called when a packet has been received by the broadcast module.

void(* broadcast_callbacks::sent)(struct broadcast_conn *ptr, int status, int num_tx)