The DSC program description structure.
The DSC structure is used for describing a Contiki program. It includes a short textual description of the program, either the name of the program on disk, or a pointer to the init() function, and an icon for the program.
#include <dsc.h>
Data Fields | |
char * | description |
A text string containing a one-line description of the program More... | |
struct process * | process |
A pointer to the program's process. More... | |
char* dsc::description |
A text string containing a one-line
description of the program
struct process* dsc::process |
A pointer to the program's process.