Microchip® Advanced Software Framework

pds_env Struct Reference

containing environment parameters of the NVM module.

#include <pds_nvm.h>

Data Fields

uint32_t flash_id
 
uint32_t pds_nvm_start_address
 
uint32_t pds_sector_count
 
uint32_t pds_sector_size
 

uint32_t pds_env::flash_id

<Id of the flash Internal/External

Referenced by pds_nvm_erase(), pds_nvm_init(), pds_nvm_read(), and pds_nvm_write().

uint32_t pds_env::pds_nvm_start_address
uint32_t pds_env::pds_sector_count

pds sector size

Referenced by pds_compact_sector(), pds_delete_all(), and pds_init().