Microchip® Advanced Software Framework

t_monitor_if Struct Reference

Data Fields

int(* getc )(void)
 
uint32_t(* getdata )(void *data, uint32_t length)
 
uint32_t(* getdata_xmd )(void *data, uint32_t length)
 
bool(* is_rx_ready )(void)
 
int(* putc )(int value)
 
uint32_t(* putdata )(void const *data, uint32_t length)
 
uint32_t(* putdata_xmd )(void const *data, uint32_t length)
 

int(* t_monitor_if::getc)(void)
uint32_t(* t_monitor_if::getdata)(void *data, uint32_t length)

Referenced by sam_ba_monitor_run().

uint32_t(* t_monitor_if::getdata_xmd)(void *data, uint32_t length)

Referenced by sam_ba_monitor_run().

bool(* t_monitor_if::is_rx_ready)(void)
int(* t_monitor_if::putc)(int value)
uint32_t(* t_monitor_if::putdata)(void const *data, uint32_t length)
uint32_t(* t_monitor_if::putdata_xmd)(void const *data, uint32_t length)

Referenced by sam_ba_monitor_run().