Microchip® Advanced Software Framework

uip_fw_netif Struct Reference

Representation of a uIP network interface.

#include <uip-fw.h>

Data Fields

uip_ipaddr_t ipaddr
 The IP address of this interface. More...
 
uip_ipaddr_t netmask
 The netmask of the interface. More...
 
struct uip_fw_netifnext
 
           Pointer to the next interface when

linked in a list. More...

 
uint8_t(* output )(void)
 
              A pointer to the function that

sends a packet. More...

 

uip_ipaddr_t uip_fw_netif::ipaddr

The IP address of this interface.

Referenced by find_netif().

uip_ipaddr_t uip_fw_netif::netmask

The netmask of the interface.

Referenced by find_netif().

struct uip_fw_netif* uip_fw_netif::next

           Pointer to the next interface when

linked in a list.

Referenced by find_netif(), uip_fw_init(), uip_fw_output(), and uip_fw_register().

uint8_t(* uip_fw_netif::output)(void)

              A pointer to the function that

sends a packet.

Referenced by uip_fw_output(), and uip_over_mesh_send().