Microchip® Advanced Software Framework

wpan_addr_spec_tag Struct Reference

Device address specification structure.

#include <mac_api.h>

Data Fields

address_field_t Addr
 Device address. More...
 
uint8_t AddrMode
 Address mode (WPAN_ADDRMODE_NONE, WPAN_ADDRMODE_SHORT, or WPAN_ADDRMODE_LONG) More...
 
uint16_t PANId
 The 16 bit PAN identifier. More...
 

address_field_t wpan_addr_spec_tag::Addr

Device address.

If AddrMode is WPAN_ADDRMODE_SHORT, it is interpreted as a 16 bit address.

Referenced by bc_data_cb(), gts_data_cb(), handle_incoming_msg(), indirect_data_cb(), main(), mcps_data_ind(), usr_mcps_data_ind(), usr_mlme_set_conf(), and wpan_mcps_data_req().

uint16_t wpan_addr_spec_tag::PANId