Heart Rate Sensor Profile declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | ADV_DATA_LEN (18) |
ADV_DATA_LEN. More... | |
#define | ADV_TYPE_LEN (0x01) |
ADV_TYPE_LEN. More... | |
#define | DEVICE_INFORMATION_SERVICE_UUID (0x180A) |
DEVICE_INFORMATION_SERVICE_UUID. More... | |
#define | FLAG_ENERGY_EXP (0x1 << 3) |
#define | HR_APP_CONNECTION_STATE (1) |
APP_CONNECTION_STATE indicates application is in connected state. More... | |
#define | HR_APP_DISCONNECT_STATE (0) |
APP_DISCONNECT_STATE indicates application is in disconnected state. More... | |
#define | HR_CONTROL_POINT_RESET_VAL (1) |
#define | HR_SENSOR_ADV_DATA_COMP_16_UUID_TYPE (0x03) |
HR_SENSOR_ADV_DATA_UUID_TYPE is complete 16 bit uuid type. More... | |
#define | HR_SENSOR_ADV_DATA_NAME_DATA ("ATMEL-HRP") |
#define | HR_SENSOR_ADV_DATA_NAME_LEN (9) |
HR_SENSOR_ADV_DATA_NAME_LEN the length of the device name. More... | |
#define | HR_SENSOR_ADV_DATA_NAME_TYPE (0x09) |
HR_SENSOR_ADV_DATA_NAME_TYPE the gap ad data type. More... | |
#define | HR_SENSOR_ADV_DATA_UUID_LEN (4) |
HR_SENSOR_ADV_DATA_UUID_LEN the total length for hr uuid and dis uuid. More... | |
#define | HR_SENSOR_ADV_TIMEOUT (655) |
APP_HR_SENSOR_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out. More... | |
#define | HR_SENSOR_FAST_ADV (1600) |
APP_HR_SENSOR_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s). More... | |
#define | SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data More... | |
#define | UUID_16_BIT_LEN (0x02) |
Typedefs | |
typedef void(* | hr_notification_callback_t )(uint8_t) |
typedef void(* | hr_reset_callback_t )(void) |
Functions | |
at_ble_status_t | hr_notification_confirmation_handler (void *params) |
register_hr_notification_handler registers the notification handler passed by the application More... | |
void | hr_sensor_adv (void) |
hr_sensor_adv adds the advertisement data of the profile and starts advertisement More... | |
at_ble_status_t | hr_sensor_char_changed_handler (void *char_params) |
hr_sensor_char_changed_handler called by the ble manager after a change in the characteristic More... | |
at_ble_status_t | hr_sensor_char_write_request (void *params) |
hr_sensor_char_write_request handles the write request for heart rate control point characteristic. More... | |
at_ble_status_t | hr_sensor_connected_state_handler (void *params) |
hr_sensor_connected_state_handler called by ble manager after a change in characteristic More... | |
void | hr_sensor_disconnect (void) |
hr_sensor_disconnect disconnects with the peer device called by the application More... | |
at_ble_status_t | hr_sensor_disconnect_event_handler (void *disconnect) |
hr_sensor_disconnect_event_handler called by ble manager after disconnection event recieved More... | |
void | hr_sensor_init (void *param) |
hr_sensor_init initializes and defines the services of the hr profile More... | |
at_ble_status_t | hr_sensor_notification_cfm_handler (void *params) |
hr_sensor_notification_cfm_handler called on notification confirmation event by the ble manager More... | |
bool | hr_sensor_send_notification (uint8_t *hr_data, uint8_t length) |
hr_sensor_send_notification adds the new characteristic value and sends the notification More... | |
void | hr_sensor_service_define (void) |
hr_sensor_service_define defines the services of the profile More... | |
void | hr_sensor_service_init (void) |
hr_sensor_service_init initializes the services of the profile More... | |
void | register_hr_notification_handler (hr_notification_callback_t hr_notificaton_handler) |
register_hr_notification_handler registers the notification handler passed by the application param[in] hr_notification_callback_t address of the notification handler function to be called More... | |
void | register_hr_reset_handler (hr_reset_callback_t hr_reset_handler) |
register_hr_reset_handler registers the reset handler passed by the application More... | |
#define ADV_DATA_LEN (18) |
ADV_DATA_LEN.
#define ADV_TYPE_LEN (0x01) |
ADV_TYPE_LEN.
#define DEVICE_INFORMATION_SERVICE_UUID (0x180A) |
DEVICE_INFORMATION_SERVICE_UUID.
#define FLAG_ENERGY_EXP (0x1 << 3) |
#define HR_APP_CONNECTION_STATE (1) |
APP_CONNECTION_STATE indicates application is in connected state.
#define HR_APP_DISCONNECT_STATE (0) |
APP_DISCONNECT_STATE indicates application is in disconnected state.
#define HR_CONTROL_POINT_RESET_VAL (1) |
Referenced by hr_sensor_char_write_request().
#define HR_SENSOR_ADV_DATA_COMP_16_UUID_TYPE (0x03) |
HR_SENSOR_ADV_DATA_UUID_TYPE is complete 16 bit uuid type.
#define HR_SENSOR_ADV_DATA_NAME_DATA ("ATMEL-HRP") |
#define HR_SENSOR_ADV_DATA_NAME_LEN (9) |
HR_SENSOR_ADV_DATA_NAME_LEN the length of the device name.
#define HR_SENSOR_ADV_DATA_NAME_TYPE (0x09) |
HR_SENSOR_ADV_DATA_NAME_TYPE the gap ad data type.
#define HR_SENSOR_ADV_DATA_UUID_LEN (4) |
HR_SENSOR_ADV_DATA_UUID_LEN the total length for hr uuid and dis uuid.
#define HR_SENSOR_ADV_TIMEOUT (655) |
APP_HR_SENSOR_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out.
#define HR_SENSOR_FAST_ADV (1600) |
APP_HR_SENSOR_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s).
Referenced by hr_sensor_adv().
#define SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data
#define UUID_16_BIT_LEN (0x02) |
typedef void(* hr_notification_callback_t)(uint8_t) |
typedef void(* hr_reset_callback_t)(void) |
at_ble_status_t hr_notification_confirmation_handler | ( | void * | params | ) |
register_hr_notification_handler registers the notification handler passed by the application
[in] | hr_notification_callback_t | address of the notification handler function to be called |
void hr_sensor_adv | ( | void | ) |
hr_sensor_adv adds the advertisement data of the profile and starts advertisement
References AT_BLE_ADV_FP_ANY, AT_BLE_ADV_GEN_DISCOVERABLE, at_ble_adv_start(), AT_BLE_ADV_TYPE_UNDIRECTED, AT_BLE_SUCCESS, DBG_LOG, HR_SENSOR_FAST_ADV, NULL, and status.
Referenced by hr_sensor_app_custom_event().
at_ble_status_t hr_sensor_char_changed_handler | ( | void * | params | ) |
hr_sensor_char_changed_handler called by the ble manager after a change in the characteristic
[in] | at_ble_characteristic_changed_t | which contains handle of characteristic and new value |
References AT_BLE_SUCCESS, HR_CONTROL_POINT_RESET, HR_NOTIFICATION_DISABLE, HR_NOTIFICATION_ENABLE, hr_write_value_handler(), notification_cb, and reset_cb.
at_ble_status_t hr_sensor_char_write_request | ( | void * | params | ) |
hr_sensor_char_write_request handles the write request for heart rate control point characteristic.
[in] | at_ble_characteristic_write_request_t | parameters containing the value written |
References AT_BLE_ATT_APP_ERROR, AT_BLE_SUCCESS, at_ble_write_authorize_reply(), at_ble_characteristic_write_request_t::char_handle, at_ble_characteristic_t::char_val_handle, DBG_LOG, DBG_LOG_DEV, HR_CONTROL_POINT_RESET_VAL, reset_cb, hr_gatt_service_handler::serv_chars, status, and at_ble_characteristic_write_request_t::value.
at_ble_status_t hr_sensor_connected_state_handler | ( | void * | params | ) |
hr_sensor_connected_state_handler called by ble manager after a change in characteristic
[in] | at_ble_connected_t | which has connection handle and the peer device address |
References AT_BLE_SUCCESS, connection_handle, and at_ble_connected_t::handle.
void hr_sensor_disconnect | ( | void | ) |
hr_sensor_disconnect disconnects with the peer device called by the application
References at_ble_disconnect(), AT_BLE_SUCCESS, AT_BLE_TERMINATED_BY_USER, connection_handle, DBG_LOG, and status.
Referenced by hr_sensor_app_custom_event().
at_ble_status_t hr_sensor_disconnect_event_handler | ( | void * | disconnect | ) |
hr_sensor_disconnect_event_handler called by ble manager after disconnection event recieved
[in] | at_ble_disconnected_t | which has connection handle and reason for disconnection |
References ALL_UNUSED, and AT_BLE_SUCCESS.
void hr_sensor_init | ( | void * | param | ) |
hr_sensor_init initializes and defines the services of the hr profile
[in] | params | are unused. |
References ALL_UNUSED, AT_BLE_SUCCESS, ble_advertisement_data_set(), BLE_GAP_EVENT_TYPE, BLE_GATT_SERVER_EVENT_TYPE, ble_mgr_events_callback_handler(), at_ble_characteristic_t::char_val_handle, at_ble_characteristic_t::client_config_handle, DBG_LOG, DBG_LOG_PTS, hr_sensor_service_define(), hr_sensor_service_init(), REGISTER_CALL_BACK, hr_gatt_service_handler::serv_chars, dis_gatt_service_handler::serv_chars, hr_gatt_service_handler::serv_handle, dis_gatt_service_handler::serv_handle, and status.
Referenced by main().
at_ble_status_t hr_sensor_notification_cfm_handler | ( | void * | params | ) |
hr_sensor_notification_cfm_handler called on notification confirmation event by the ble manager
[in] | at_ble_status_t | AT_BLE_SUCCESS on success AT_BLE_FAILURE on failure called |
hr_sensor_notification_cfm_handler called on notification confirmation event by the ble manager
[in] | at_ble_status_t | AT_BLE_SUCCESS on success AT_BLE_FAILURE on failure called |
References AT_BLE_SUCCESS, DBG_LOG_DEV, and at_ble_cmd_complete_event_t::status.
bool hr_sensor_send_notification | ( | uint8_t * | hr_data, |
uint8_t | length | ||
) |
hr_sensor_send_notification adds the new characteristic value and sends the notification
[in] | hr_data | the new hr characteristic value needs to be updated |
[in] | length | length of new characteristic value |
[in] | hr_data | the new hr characteristic value needs to be updated |
[in] | length | length of new characteristic value |
Updating the new characteristic value
Sending the notification for the updated characteristic
References at_ble_characteristic_value_set(), at_ble_notification_send(), AT_BLE_SUCCESS, at_ble_characteristic_t::char_val_handle, connection_handle, DBG_LOG, hr_gatt_service_handler::serv_chars, and status.
Referenced by hr_measurment_send().
void hr_sensor_service_define | ( | void | ) |
hr_sensor_service_define defines the services of the profile
References AT_BLE_SUCCESS, DBG_LOG, DBG_LOG_DEV, dis_primary_service_define(), hr_primary_service_define(), and status.
Referenced by hr_sensor_init().
void hr_sensor_service_init | ( | void | ) |
hr_sensor_service_init initializes the services of the profile
hr_sensor_service_init initializes the services of the profile
References dis_init_service(), and hr_init_service().
Referenced by hr_sensor_init().
void register_hr_notification_handler | ( | hr_notification_callback_t | hr_notificaton_handler | ) |
register_hr_notification_handler registers the notification handler passed by the application param[in] hr_notification_callback_t address of the notification handler function to be called
References notification_cb.
Referenced by main().
void register_hr_reset_handler | ( | hr_reset_callback_t | hr_reset_handler | ) |