Link Loss Service declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
#include "at_ble_api.h"
#include "ble_utils.h"
#include "ble_manager.h"
Data Structures | |
struct | gatt_lls_char_handler |
struct | gatt_lls_char_handler |
Macros | |
#define | INVALID_LLS_PARAM (0xff) |
#define | LLS_ALERT_LEVEL LLS_HIGH_ALERT |
#define | LLS_CHARACTERISTIC_COUNT (1) |
count of characteristics in linkloss service More... | |
#define | LLS_CLIENT 0 |
#define | LLS_INCLUDED_SERVICE_COUNT (0) |
count of included service in Linkloss service More... | |
#define | LLS_INVALID_CHAR_HANDLE (0) |
#define | LLS_LEVEL (2) |
#define | LLS_NO_SIGNED_WRITE (false) |
#define | LLS_READ_LENGTH (1) |
#define | LLS_READ_OFFSET (0) |
#define | LLS_READ_RESP_INVALID (-1) |
#define | LLS_SERVER 0 |
#define | LLS_WRITE_LENGTH (1) |
#define | LLS_WRITE_OFFSET (0) |
#define | LLS_WRITE_WITH_RESPONSE (true) |
#define | MAX_LLS_CHAR_SIZE (1) |
Typedefs | |
typedef struct gatt_lls_char_handler | gatt_lls_char_handler_t |
typedef enum linkloss_alert_level | linkloss_alert_level_t |
Enumerations | |
enum | link_loss_alert_level_t { LLS_NO_ALERT, LLS_MILD_ALERT, LLS_HIGH_ALERT, LLS_NO_ALERT, LLS_LOW_ALERT, LLS_HIGH_ALERT } |
enum | linkloss_alert_level { LLS_NO_ALERT, LLS_MILD_ALERT, LLS_HIGH_ALERT, LLS_NO_ALERT, LLS_MILD_ALERT, LLS_HIGH_ALERT } |
Functions | |
void | init_linkloss_service (gatt_service_handler_t *linkloss_serv) |
Initialize the linkloss service with default values. More... | |
at_ble_status_t | lls_alert_level_read (at_ble_handle_t conn_handle, at_ble_handle_t char_handle) |
Send the Read request to link loss handler Read value will be reported via AT_BLE_CHARACTERISTIC_READ_RESPONSE event. More... | |
at_ble_status_t | lls_alert_level_write (at_ble_handle_t conn_handle, at_ble_handle_t char_handle, link_loss_alert_level_t alert_level) |
write a characteristic to Link Loss Characteristics More... | |
int8_t | lls_alert_read_response (at_ble_characteristic_read_response_t *read_resp, gatt_lls_char_handler_t *lls_handler) |
Read Link Loss Alert Value. More... | |
at_ble_status_t | lls_primary_service_define (gatt_service_handler_t *lls_service) |
Defining linkloss service to the attribute data base. More... | |
uint8_t | lls_set_alert_value (at_ble_characteristic_changed_t *change_params, gatt_service_handler_t *lls_handler) |
sets the alert value of the Linkloss service More... | |
#define INVALID_LLS_PARAM (0xff) |
Referenced by lls_set_alert_value(), and pxp_reporter_char_changed_handler().
#define LLS_ALERT_LEVEL LLS_HIGH_ALERT |
Referenced by pxp_monitor_discovery_complete_handler().
#define LLS_CHARACTERISTIC_COUNT (1) |
count of characteristics in linkloss service
Referenced by lls_primary_service_define().
#define LLS_CLIENT 0 |
#define LLS_INCLUDED_SERVICE_COUNT (0) |
count of included service in Linkloss service
Referenced by lls_primary_service_define().
#define LLS_INVALID_CHAR_HANDLE (0) |
Referenced by lls_alert_level_read().
#define LLS_LEVEL (2) |
#define LLS_NO_SIGNED_WRITE (false) |
Referenced by lls_alert_level_write().
#define LLS_READ_LENGTH (1) |
Referenced by lls_alert_level_read(), and lls_alert_read_response().
#define LLS_READ_OFFSET (0) |
Referenced by lls_alert_level_read(), and lls_alert_read_response().
#define LLS_READ_RESP_INVALID (-1) |
Referenced by lls_alert_read_response().
#define LLS_SERVER 0 |
#define LLS_WRITE_LENGTH (1) |
Referenced by lls_alert_level_write().
#define LLS_WRITE_OFFSET (0) |
Referenced by lls_alert_level_write().
#define LLS_WRITE_WITH_RESPONSE (true) |
Referenced by lls_alert_level_write().
#define MAX_LLS_CHAR_SIZE (1) |
typedef enum linkloss_alert_level linkloss_alert_level_t |
enum linkloss_alert_level |
void init_linkloss_service | ( | gatt_service_handler_t * | linkloss_serv | ) |
Initialize the linkloss service with default values.
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
Initialize the linkloss service with default values.
at_ble_status_t lls_alert_level_read | ( | at_ble_handle_t | conn_handle, |
at_ble_handle_t | char_handle | ||
) |
Send the Read request to link loss handler Read value will be reported via AT_BLE_CHARACTERISTIC_READ_RESPONSE event.
[in] | conn_handle | handle of the connection |
[in] | char_handle | handle of the characteristic |
Send the Read request to link loss handler Read value will be reported via AT_BLE_CHARACTERISTIC_READ_RESPONSE event.
[in] | conn_handle | handle of the connection |
[in] | char_handle | handle of the characteristic |
at_ble_status_t lls_alert_level_write | ( | at_ble_handle_t | conn_handle, |
at_ble_handle_t | char_handle, | ||
link_loss_alert_level_t | alert_level | ||
) |
write a characteristic to Link Loss Characteristics
if with_response is True, write completion will be reported via AT_BLE_CHARACTERISTIC_WRITE_RESPONSE event
[in] | conn_handle | handle of the connection |
[in] | char_handle | handle of the characteristic |
[in] | alert | level need to write |
int8_t lls_alert_read_response | ( | at_ble_characteristic_read_response_t * | read_resp, |
gatt_lls_char_handler_t * | lls_handler | ||
) |
Read Link Loss Alert Value.
[in] | read_value | read response data available form at_ble_characteristic_read_response_t |
[in] | read_value | read response data available form at_ble_characteristic_read_response_t |
at_ble_status_t lls_primary_service_define | ( | gatt_service_handler_t * | lls_service | ) |
Defining linkloss service to the attribute data base.
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
Defining linkloss service to the attribute data base.
uint8_t lls_set_alert_value | ( | at_ble_characteristic_changed_t * | change_params, |
gatt_service_handler_t * | lls_handler | ||
) |
sets the alert value of the Linkloss service
[in] | gatt_service_handler_t | the service info which has handle range,uuid and characteristic array fields |
[in] | at_ble_characteristic_changed_t | the information of the characteristic changed. |
sets the alert value of the Linkloss service