Declaration of main function.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include "uhc.h"
Functions | |
void | main_usb_connection_event (uhc_device_t *dev, bool b_present) |
Notify that a USB device has been connected or disconnected. More... | |
void | main_usb_enum_event (uhc_device_t *dev, uhc_enum_status_t status) |
Notify the end of a USB device enumeration. More... | |
void | main_usb_mode_change (bool b_host_mode) |
Notify that the USB mode was automatically switched. This is possible only when ID pin is available. More... | |
void | main_usb_sof_event (void) |
Notify that a SOF has been sent (each 1 ms) More... | |
void | main_usb_vbus_change (bool b_vbus_present) |
Notify that a Vbus transition has occurred Available only in USB hardware with Vbus monitoring. More... | |
void | main_usb_vbus_error (void) |
Notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring. More... | |
void | main_usb_wakeup_event (void) |
Notify that a USB device or the host has wake up the USB line. More... | |
void main_usb_connection_event | ( | uhc_device_t * | dev, |
bool | b_present | ||
) |
Notify that a USB device has been connected or disconnected.
dev | Pointer on USB device information |
b_present | true, if the device has been connected |
Notify that a USB device has been connected or disconnected.
void main_usb_enum_event | ( | uhc_device_t * | dev, |
uhc_enum_status_t | status | ||
) |
Notify the end of a USB device enumeration.
dev | Pointer on USB device information |
status | Status of the USB enumeration |
Device is bus enumerated with at least one supported interface
All interfaces are not supported by UHIs
Device power can not be supported
A problem has been occurred during USB enumeration
USB hardware can not support it. Not enough free pipes.
References MAIN_EVENT_ENUM_FAIL, MAIN_EVENT_ENUM_HARDWARE_LIMIT, MAIN_EVENT_ENUM_OVERCURRENT, MAIN_EVENT_ENUM_SUCCESS_FULL_SPEEP, MAIN_EVENT_ENUM_SUCCESS_HIGH_SPEEP, MAIN_EVENT_ENUM_SUCCESS_LOW_SPEEP, MAIN_EVENT_ENUM_UNKNOW, MAIN_EVENT_ENUM_UNSUPPORTED, main_events, uhc_device_t::speed, UHC_ENUM_FAIL, UHC_ENUM_HARDWARE_LIMIT, UHC_ENUM_OVERCURRENT, UHC_ENUM_SUCCESS, UHC_ENUM_UNSUPPORTED, UHD_SPEED_FULL, UHD_SPEED_HIGH, and UHD_SPEED_LOW.
void main_usb_mode_change | ( | bool | b_host_mode | ) |
Notify that the USB mode was automatically switched. This is possible only when ID pin is available.
b_host_mode | true, if the host mode has been selected |
References MAIN_EVENT_DEVICE_MODE, MAIN_EVENT_HOST_MODE, and main_events.
void main_usb_sof_event | ( | void | ) |
Notify that a SOF has been sent (each 1 ms)
void main_usb_vbus_change | ( | bool | b_vbus_present | ) |
Notify that a Vbus transition has occurred Available only in USB hardware with Vbus monitoring.
b_vbus_present | true, if Vbus is high. |
References MAIN_EVENT_VBUS_NOT_PRESENT, MAIN_EVENT_VBUS_PRESENT, and main_events.
void main_usb_vbus_error | ( | void | ) |
Notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring.
void main_usb_wakeup_event | ( | void | ) |
Notify that a USB device or the host has wake up the USB line.
References MAIN_EVENT_WAKEUP, and main_events.