Microchip® Advanced Software Framework

winc1500/mac_address_example/main21.c File Reference

WINC1500 MAC Address Example.

Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.

#include "asf.h"
#include "driver/include/m2m_wifi.h"
#include "driver/source/nmasic.h"

Macros

#define STRING_EOL   "\r\n"
 
#define STRING_HEADER
 

Functions

static void configure_console (void)
 Configure UART console. More...
 
int main (void)
 Main application function. More...
 

Variables

static struct usart_module cdc_uart_module
 UART module for debug. More...
 
static uint8_t mac_addr [M2M_MAC_ADDRES_LEN]
 Mac address information. More...
 
const char main_user_define_mac_address [] = {0xf8, 0xf0, 0x05, 0x20, 0x0b, 0x09}
 User define MAC Address. More...
 

#define STRING_EOL   "\r\n"
#define STRING_HEADER
Value:
"-- WINC1500 MAC Address example --"STRING_EOL \
"-- "BOARD_NAME " --"STRING_EOL \
"-- Compiled: "__DATE__ " "__TIME__ " --"STRING_EOL
#define BOARD_NAME
Definition: app_init.h:140
#define STRING_EOL
Definition: winc1500/mac_address_example/main21.c:80

Referenced by main().

int main ( void  )

Main application function.

Application entry point. Initialize board and WINC1500 Wi-Fi module.

Returns
program return value.

References configure_console(), M2M_SUCCESS, m2m_wifi_get_mac_address(), m2m_wifi_get_otp_mac_address(), m2m_wifi_init(), m2m_wifi_set_mac_address(), mac_addr, main_user_define_mac_address, nm_bsp_init(), printf, ret, STRING_HEADER, and system_init().

struct usart_module cdc_uart_module
static

UART module for debug.

uint8_t mac_addr[M2M_MAC_ADDRES_LEN]
static

Mac address information.

Referenced by main().

const char main_user_define_mac_address[] = {0xf8, 0xf0, 0x05, 0x20, 0x0b, 0x09}

User define MAC Address.

Referenced by main().