Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an TaskHandle_t variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Fri Mar 4 2022 23:46:56 for SAML21 by 1.8.5