This is the MLME-BEACON-NOTIFY.indication message structure.
#include <mac_msg_types.h>
Data Fields | |
uint8_t * | AddrList |
The list of addresses of the devices for which the beacon source has data. More... | |
uint8_t | BSN |
The beacon sequence number. More... | |
enum msg_code | cmdcode |
This identifies the message as MLME_BEACON_NOTIFY_INDICATION. More... | |
wpan_pandescriptor_t | PANDescriptor |
The PANDescriptor for the received beacon. More... | |
uint8_t | PendAddrSpec |
The beacon pending address specification. More... | |
uint8_t * | sdu |
The set of octets comprising the beacon payload to be transferred from the MAC sublayerentity to the next higher layer. More... | |
uint8_t | sduLength |
The number of octets contained in the beacon payload of the beacon frame received by the MAC sublayer. More... | |