This is the MLME-COMM-STATUS.indication message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
This identifies the message as MLME_COMM_STATUS_INDICATION. More... | |
uint64_t | DstAddr |
The individual device address of the device for which the frame was intended. More... | |
uint8_t | DstAddrMode |
The destination addressing mode for this primitive. More... | |
uint16_t | PANId |
The 16 bit PAN identifier of the device from which the frame was received or to which the frame was being sent. More... | |
uint64_t | SrcAddr |
The source addressing mode for this primitive. More... | |
uint8_t | SrcAddrMode |
The source addressing mode for this primitive. More... | |
uint8_t | status |
The communications status. More... | |