This is the MLME-ORPHAN.response message structure.
#include <mac_msg_types.h>
Data Fields | |
uint8_t | AssociatedMember |
TRUE if the orphaned device is associated with this coordinator or FALSE otherwise. More... | |
enum msg_code | cmdcode |
This identifies the message as MLME_ORPHAN_RESPONSE. More... | |
uint64_t | OrphanAddress |
The address of the orphaned device. More... | |
uint16_t | ShortAddress |
The short address allocated to the orphaned device if it is associated with this coordinator. More... | |