This is the MLME-RX-ENABLE.request message structure.
#include <mac_msg_types.h>
Data Fields | |
enum msg_code | cmdcode |
This identifies the message as MLME_RX_ENABLE_REQUEST. More... | |
uint8_t | DeferPermit |
TRUE if the receiver enable can be deferred until during the next superframe if the requested time has already passed. More... | |
uint32_t | RxOnDuration |
The number of symbols for which the receiver is to be enabled. More... | |
uint32_t | RxOnTime |
The number of symbols from the start of the superframe before the receiver is to be enabled. More... | |