This is the MLME-SYNC-LOSS.indication message structure.
#include <mac_msg_types.h>
Data Fields | |
uint8_t | ChannelPage |
The channel page on which the device lost synchronization or to which it was realigned. More... | |
enum msg_code | cmdcode |
This identifies the message as MLME_SYNC_LOSS_INDICATION. More... | |
uint8_t | LogicalChannel |
The logical channel on which the device lost synchronization or to which it was realigned. More... | |
uint8_t | LossReason |
The reason that synchronization was lost. More... | |
uint16_t | PANId |
The PAN identifier with which the device lost synchronization or to which it was realigned. More... | |