Microchip® Advanced Software Framework

GFX Mono Font Example

Introduction

This is an example application for the GFX Mono Font Library. It will print a string, with line break, on the screen and scroll it.

Main files:

Device Info

This example has been tested with the following setup:

  • SAM D20 Xplained Pro
  • SAM D21 Xplained Pro
  • SAM R21 Xplained Pro
  • SAM D11 Xplained Pro
  • SAM L21 Xplained Pro
  • SAM L22 Xplained Pro

Description of the example application

The example application will upon power up display several text strings on the display; "PASSION...".

Dependencies

Relevant module dependencies for this application are:

Compilation info

This software was written for the GNU GCC and IAR. Other compilers may or may not work.

Contact Information

For further information, visit Microchip.